Used in the SD24_initConverterAdvanced() function as the param parameter. More...
#include <sd24.h>
Data Fields | |
uint8_t | converter |
uint16_t | conversionMode |
uint8_t | groupEnable |
uint8_t | inputChannel |
uint8_t | dataFormat |
uint8_t | interruptDelay |
uint16_t | oversampleRatio |
uint8_t | gain |
Used in the SD24_initConverterAdvanced() function as the param parameter.
uint16_t SD24_initConverterAdvancedParam::conversionMode |
Determines whether the converter will do continuous samples or a single sample
Valid values are:
Referenced by SD24_initConverterAdvanced().
uint8_t SD24_initConverterAdvancedParam::converter |
Selects the converter that will be configured. Check check datasheet for available converters on device.
Valid values are:
Referenced by SD24_initConverterAdvanced().
uint8_t SD24_initConverterAdvancedParam::dataFormat |
Selects how the data format of the results
Valid values are:
Referenced by SD24_initConverterAdvanced().
uint8_t SD24_initConverterAdvancedParam::gain |
Selects the gain for the converter
Valid values are:
Referenced by SD24_initConverterAdvanced().
uint8_t SD24_initConverterAdvancedParam::groupEnable |
Valid values are:
Referenced by SD24_initConverterAdvanced().
uint8_t SD24_initConverterAdvancedParam::inputChannel |
Selects oversampling ratio for the converter
Valid values are:
Referenced by SD24_initConverterAdvanced().
uint8_t SD24_initConverterAdvancedParam::interruptDelay |
Selects the delay for the interrupt
Valid values are:
Referenced by SD24_initConverterAdvanced().
uint16_t SD24_initConverterAdvancedParam::oversampleRatio |
Selects oversampling ratio for the converter
Valid values are:
Referenced by SD24_initConverterAdvanced().