Used in the EUSCI_B_SPI_initSlave() function as the param parameter. More...
#include <eusci_b_spi.h>
Data Fields | |
uint16_t | msbFirst |
uint16_t | clockPhase |
uint16_t | clockPolarity |
uint16_t | spiMode |
Used in the EUSCI_B_SPI_initSlave() function as the param parameter.
uint16_t EUSCI_B_SPI_initSlaveParam::clockPhase |
Is clock phase select.
Valid values are:
Referenced by EUSCI_B_SPI_initSlave().
uint16_t EUSCI_B_SPI_initSlaveParam::clockPolarity |
Is clock polarity select
Valid values are:
Referenced by EUSCI_B_SPI_initSlave().
uint16_t EUSCI_B_SPI_initSlaveParam::msbFirst |
Controls the direction of the receive and transmit shift register.
Valid values are:
Referenced by EUSCI_B_SPI_initSlave().
uint16_t EUSCI_B_SPI_initSlaveParam::spiMode |
Is SPI mode select
Valid values are:
Referenced by EUSCI_B_SPI_initSlave().