Used in the EUSCI_A_UART_init() function as the param parameter. More...
#include <eusci_a_uart.h>
Data Fields | |
uint8_t | selectClockSource |
uint16_t | clockPrescalar |
Is the value to be written into UCBRx bits. | |
uint8_t | firstModReg |
uint8_t | secondModReg |
uint8_t | parity |
uint16_t | msborLsbFirst |
uint16_t | numberofStopBits |
uint16_t | uartMode |
uint8_t | overSampling |
Used in the EUSCI_A_UART_init() function as the param parameter.
uint8_t EUSCI_A_UART_initParam::firstModReg |
Is First modulation stage register setting. This value is a pre- calculated value which can be obtained from the Device Users Guide. This value is written into UCBRFx bits of UCAxMCTLW.
Referenced by EUSCI_A_UART_init().
uint16_t EUSCI_A_UART_initParam::msborLsbFirst |
Controls direction of receive and transmit shift register.
Valid values are:
Referenced by EUSCI_A_UART_init().
uint16_t EUSCI_A_UART_initParam::numberofStopBits |
Indicates one/two STOP bits
Valid values are:
Referenced by EUSCI_A_UART_init().
uint8_t EUSCI_A_UART_initParam::overSampling |
Indicates low frequency or oversampling baud generation
Valid values are:
Referenced by EUSCI_A_UART_init().
uint8_t EUSCI_A_UART_initParam::parity |
Is the desired parity.
Valid values are:
Referenced by EUSCI_A_UART_init().
uint8_t EUSCI_A_UART_initParam::secondModReg |
Is Second modulation stage register setting. This value is a pre- calculated value which can be obtained from the Device Users Guide. This value is written into UCBRSx bits of UCAxMCTLW.
Referenced by EUSCI_A_UART_init().
uint8_t EUSCI_A_UART_initParam::selectClockSource |
Selects Clock source.
Valid values are:
Referenced by EUSCI_A_UART_init().
uint16_t EUSCI_A_UART_initParam::uartMode |
Selects the mode of operation
Valid values are:
Referenced by EUSCI_A_UART_init().