Used in the Timer_A_initUpMode() function as the param parameter. More...
#include <timer_a.h>
Data Fields | |
uint16_t | clockSource |
uint16_t | clockSourceDivider |
uint16_t | timerPeriod |
uint16_t | timerInterruptEnable_TAIE |
uint16_t | captureCompareInterruptEnable_CCR0_CCIE |
uint16_t | timerClear |
bool | startTimer |
Whether to start the timer immediately. | |
Used in the Timer_A_initUpMode() function as the param parameter.
uint16_t Timer_A_initUpModeParam::captureCompareInterruptEnable_CCR0_CCIE |
Is to enable or disable Timer_A CCR0 captureComapre interrupt.
Valid values are:
Referenced by Timer_A_initUpMode().
uint16_t Timer_A_initUpModeParam::clockSource |
Selects Clock source.
Valid values are:
Referenced by Timer_A_initUpMode().
uint16_t Timer_A_initUpModeParam::clockSourceDivider |
Is the desired divider for the clock source
Valid values are:
Referenced by Timer_A_initUpMode().
uint16_t Timer_A_initUpModeParam::timerClear |
Decides if Timer_A clock divider, count direction, count need to be reset.
Valid values are:
Referenced by Timer_A_initUpMode().
uint16_t Timer_A_initUpModeParam::timerInterruptEnable_TAIE |
Is to enable or disable Timer_A interrupt
Valid values are:
Referenced by Timer_A_initUpMode().
uint16_t Timer_A_initUpModeParam::timerPeriod |
Is the specified Timer_A period. This is the value that gets written into the CCR0. Limited to 16 bits[uint16_t]
Referenced by Timer_A_initUpMode().