Used in the ADC12_B_configureMemory() function as the param parameter.
More...
#include <adc12_b.h>
Used in the ADC12_B_configureMemory() function as the param parameter.
uint16_t ADC12_B_configureMemoryParam::differentialModeSelect |
Sets the differential mode
Valid values are:
- ADC12_B_DIFFERENTIAL_MODE_DISABLE [Default]
- ADC12_B_DIFFERENTIAL_MODE_ENABLE
Referenced by ADC12_B_configureMemory().
uint16_t ADC12_B_configureMemoryParam::endOfSequence |
Indicates that the specified memory buffer will be the end of the sequence if a sequenced conversion mode is selected
Valid values are:
- ADC12_B_NOTENDOFSEQUENCE [Default]
- ADC12_B_ENDOFSEQUENCE
Referenced by ADC12_B_configureMemory().
uint8_t ADC12_B_configureMemoryParam::inputSourceSelect |
Is the input that will store the converted data into the specified memory buffer.
Valid values are:
- ADC12_B_INPUT_A0 [Default]
- ADC12_B_INPUT_A1
- ADC12_B_INPUT_A2
- ADC12_B_INPUT_A3
- ADC12_B_INPUT_A4
- ADC12_B_INPUT_A5
- ADC12_B_INPUT_A6
- ADC12_B_INPUT_A7
- ADC12_B_INPUT_A8
- ADC12_B_INPUT_A9
- ADC12_B_INPUT_A10
- ADC12_B_INPUT_A11
- ADC12_B_INPUT_A12
- ADC12_B_INPUT_A13
- ADC12_B_INPUT_A14
- ADC12_B_INPUT_A15
- ADC12_B_INPUT_A16
- ADC12_B_INPUT_A17
- ADC12_B_INPUT_A18
- ADC12_B_INPUT_A19
- ADC12_B_INPUT_A20
- ADC12_B_INPUT_A21
- ADC12_B_INPUT_A22
- ADC12_B_INPUT_A23
- ADC12_B_INPUT_A24
- ADC12_B_INPUT_A25
- ADC12_B_INPUT_A26
- ADC12_B_INPUT_A27
- ADC12_B_INPUT_A28
- ADC12_B_INPUT_A29
- ADC12_B_INPUT_TCMAP
- ADC12_B_INPUT_BATMAP
Referenced by ADC12_B_configureMemory().
uint8_t ADC12_B_configureMemoryParam::memoryBufferControlIndex |
Is the selected memory buffer to set the configuration for.
Valid values are:
- ADC12_B_MEMORY_0
- ADC12_B_MEMORY_1
- ADC12_B_MEMORY_2
- ADC12_B_MEMORY_3
- ADC12_B_MEMORY_4
- ADC12_B_MEMORY_5
- ADC12_B_MEMORY_6
- ADC12_B_MEMORY_7
- ADC12_B_MEMORY_8
- ADC12_B_MEMORY_9
- ADC12_B_MEMORY_10
- ADC12_B_MEMORY_11
- ADC12_B_MEMORY_12
- ADC12_B_MEMORY_13
- ADC12_B_MEMORY_14
- ADC12_B_MEMORY_15
- ADC12_B_MEMORY_16
- ADC12_B_MEMORY_17
- ADC12_B_MEMORY_18
- ADC12_B_MEMORY_19
- ADC12_B_MEMORY_20
- ADC12_B_MEMORY_21
- ADC12_B_MEMORY_22
- ADC12_B_MEMORY_23
- ADC12_B_MEMORY_24
- ADC12_B_MEMORY_25
- ADC12_B_MEMORY_26
- ADC12_B_MEMORY_27
- ADC12_B_MEMORY_28
- ADC12_B_MEMORY_29
- ADC12_B_MEMORY_30
- ADC12_B_MEMORY_31
Referenced by ADC12_B_configureMemory().
uint16_t ADC12_B_configureMemoryParam::refVoltageSourceSelect |
Is the reference voltage source to set as the upper/lower limits for the conversion stored in the specified memory.
Valid values are:
- ADC12_B_VREFPOS_AVCC_VREFNEG_VSS [Default]
- ADC12_B_VREFPOS_INTBUF_VREFNEG_VSS
- ADC12_B_VREFPOS_EXTNEG_VREFNEG_VSS
- ADC12_B_VREFPOS_EXTBUF_VREFNEG_VSS
- ADC12_B_VREFPOS_EXTPOS_VREFNEG_VSS
- ADC12_B_VREFPOS_AVCC_VREFNEG_EXTBUF
- ADC12_B_VREFPOS_AVCC_VREFNEG_EXTPOS
- ADC12_B_VREFPOS_INTBUF_VREFNEG_EXTPOS
- ADC12_B_VREFPOS_AVCC_VREFNEG_INTBUF
- ADC12_B_VREFPOS_EXTPOS_VREFNEG_INTBUF
- ADC12_B_VREFPOS_AVCC_VREFNEG_EXTNEG
- ADC12_B_VREFPOS_INTBUF_VREFNEG_EXTNEG
- ADC12_B_VREFPOS_EXTPOS_VREFNEG_EXTNEG
- ADC12_B_VREFPOS_EXTBUF_VREFNEG_EXTNEG
Referenced by ADC12_B_configureMemory().
uint16_t ADC12_B_configureMemoryParam::windowComparatorSelect |
Sets the window comparator mode
Valid values are:
- ADC12_B_WINDOW_COMPARATOR_DISABLE [Default]
- ADC12_B_WINDOW_COMPARATOR_ENABLE
Referenced by ADC12_B_configureMemory().
The documentation for this struct was generated from the following file: