Used in the Timer_A_outputPWM() function as the param parameter. More...
#include <timer_a.h>
Data Fields | |
uint16_t | clockSource |
uint16_t | clockSourceDivider |
uint16_t | timerPeriod |
Selects the desired timer period. | |
uint16_t | compareRegister |
uint16_t | compareOutputMode |
uint16_t | dutyCycle |
Specifies the dutycycle for the generated waveform. | |
Used in the Timer_A_outputPWM() function as the param parameter.
uint16_t Timer_A_outputPWMParam::clockSource |
Selects Clock source.
Valid values are:
Referenced by Timer_A_outputPWM().
uint16_t Timer_A_outputPWMParam::clockSourceDivider |
Is the desired divider for the clock source
Valid values are:
Referenced by Timer_A_outputPWM().
uint16_t Timer_A_outputPWMParam::compareOutputMode |
Specifies the output mode.
Valid values are:
Referenced by Timer_A_outputPWM().
uint16_t Timer_A_outputPWMParam::compareRegister |
Selects the compare register being used. Refer to datasheet to ensure the device has the capture compare register being used.
Valid values are:
Referenced by Timer_A_outputPWM().