Used in the LCD_E_init() function as the initParams parameter.
More...
#include <lcd_e.h>
Used in the LCD_E_init() function as the initParams parameter.
uint16_t LCD_E_initParam::clockDivider |
Selects the divider for LCD_E frequency.
Valid values are:
- LCD_E_CLOCKDIVIDER_1 [Default]
- LCD_E_CLOCKDIVIDER_2
- LCD_E_CLOCKDIVIDER_3
- LCD_E_CLOCKDIVIDER_4
- LCD_E_CLOCKDIVIDER_5
- LCD_E_CLOCKDIVIDER_6
- LCD_E_CLOCKDIVIDER_7
- LCD_E_CLOCKDIVIDER_8
- LCD_E_CLOCKDIVIDER_9
- LCD_E_CLOCKDIVIDER_10
- LCD_E_CLOCKDIVIDER_11
- LCD_E_CLOCKDIVIDER_12
- LCD_E_CLOCKDIVIDER_13
- LCD_E_CLOCKDIVIDER_14
- LCD_E_CLOCKDIVIDER_15
- LCD_E_CLOCKDIVIDER_16
- LCD_E_CLOCKDIVIDER_17
- LCD_E_CLOCKDIVIDER_18
- LCD_E_CLOCKDIVIDER_19
- LCD_E_CLOCKDIVIDER_20
- LCD_E_CLOCKDIVIDER_21
- LCD_E_CLOCKDIVIDER_22
- LCD_E_CLOCKDIVIDER_23
- LCD_E_CLOCKDIVIDER_24
- LCD_E_CLOCKDIVIDER_25
- LCD_E_CLOCKDIVIDER_26
- LCD_E_CLOCKDIVIDER_27
- LCD_E_CLOCKDIVIDER_28
- LCD_E_CLOCKDIVIDER_29
- LCD_E_CLOCKDIVIDER_30
- LCD_E_CLOCKDIVIDER_31
- LCD_E_CLOCKDIVIDER_32
Referenced by LCD_E_init().
uint16_t LCD_E_initParam::clockSource |
Selects the clock that will be used by the LCD_E.
Valid values are:
- LCD_E_CLOCKSOURCE_XTCLK [Default]
- LCD_E_CLOCKSOURCE_ACLK [Default]
- LCD_E_CLOCKSOURCE_VLOCLK
Referenced by LCD_E_init().
uint16_t LCD_E_initParam::muxRate |
Selects LCD_E mux rate.
Valid values are:
- LCD_E_STATIC [Default]
- LCD_E_2_MUX
- LCD_E_3_MUX
- LCD_E_4_MUX
- LCD_E_5_MUX
- LCD_E_6_MUX
- LCD_E_7_MUX
- LCD_E_8_MUX
Referenced by LCD_E_init().
uint16_t LCD_E_initParam::segments |
Sets LCD segment on/off.
Valid values are:
- LCD_E_SEGMENTS_DISABLED [Default]
- LCD_E_SEGMENTS_ENABLED
Referenced by LCD_E_init().
uint16_t LCD_E_initParam::waveforms |
Selects LCD waveform mode.
Valid values are:
- LCD_E_STANDARD_WAVEFORMS [Default]
- LCD_E_LOW_POWER_WAVEFORMS
Referenced by LCD_E_init().
The documentation for this struct was generated from the following file: