Functions | |
void | CRC_setSeed (uint16_t baseAddress, uint16_t seed) |
Sets the seed for the CRC. More... | |
void | CRC_set16BitData (uint16_t baseAddress, uint16_t dataIn) |
Sets the 16 bit data to add into the CRC module to generate a new signature. More... | |
void | CRC_set8BitData (uint16_t baseAddress, uint8_t dataIn) |
Sets the 8 bit data to add into the CRC module to generate a new signature. More... | |
void | CRC_set16BitDataReversed (uint16_t baseAddress, uint16_t dataIn) |
Translates the 16 bit data by reversing the bits in each byte and then sets this data to add into the CRC module to generate a new signature. More... | |
void | CRC_set8BitDataReversed (uint16_t baseAddress, uint8_t dataIn) |
Translates the 8 bit data by reversing the bits in each byte and then sets this data to add into the CRC module to generate a new signature. More... | |
uint16_t | CRC_getData (uint16_t baseAddress) |
Returns the value currently in the Data register. More... | |
uint16_t | CRC_getResult (uint16_t baseAddress) |
Returns the value pf the Signature Result. More... | |
uint16_t | CRC_getResultBitsReversed (uint16_t baseAddress) |
Returns the bit-wise reversed format of the Signature Result. More... | |
uint16_t CRC_getData | ( | uint16_t | baseAddress | ) |
Returns the value currently in the Data register.
This function returns the value currently in the data register. If set in byte bits reversed format, then the translated data would be returned.
baseAddress | is the base address of the CRC module. |
uint16_t CRC_getResult | ( | uint16_t | baseAddress | ) |
Returns the value pf the Signature Result.
This function returns the value of the signature result generated by the CRC.
baseAddress | is the base address of the CRC module. |
uint16_t CRC_getResultBitsReversed | ( | uint16_t | baseAddress | ) |
Returns the bit-wise reversed format of the Signature Result.
This function returns the bit-wise reversed format of the Signature Result.
baseAddress | is the base address of the CRC module. |
void CRC_set16BitData | ( | uint16_t | baseAddress, |
uint16_t | dataIn | ||
) |
Sets the 16 bit data to add into the CRC module to generate a new signature.
This function sets the given data into the CRC module to generate the new signature from the current signature and new data.
baseAddress | is the base address of the CRC module. |
dataIn | is the data to be added, through the CRC module, to the signature. Modified bits are CRCDI of CRCDI register. |
void CRC_set16BitDataReversed | ( | uint16_t | baseAddress, |
uint16_t | dataIn | ||
) |
Translates the 16 bit data by reversing the bits in each byte and then sets this data to add into the CRC module to generate a new signature.
This function first reverses the bits in each byte of the data and then generates the new signature from the current signature and new translated data.
baseAddress | is the base address of the CRC module. |
dataIn | is the data to be added, through the CRC module, to the signature. Modified bits are CRCDIRB of CRCDIRB register. |
void CRC_set8BitData | ( | uint16_t | baseAddress, |
uint8_t | dataIn | ||
) |
Sets the 8 bit data to add into the CRC module to generate a new signature.
This function sets the given data into the CRC module to generate the new signature from the current signature and new data.
baseAddress | is the base address of the CRC module. |
dataIn | is the data to be added, through the CRC module, to the signature. Modified bits are CRCDI of CRCDI register. |
void CRC_set8BitDataReversed | ( | uint16_t | baseAddress, |
uint8_t | dataIn | ||
) |
Translates the 8 bit data by reversing the bits in each byte and then sets this data to add into the CRC module to generate a new signature.
This function first reverses the bits in each byte of the data and then generates the new signature from the current signature and new translated data.
baseAddress | is the base address of the CRC module. |
dataIn | is the data to be added, through the CRC module, to the signature. Modified bits are CRCDIRB of CRCDIRB register. |
void CRC_setSeed | ( | uint16_t | baseAddress, |
uint16_t | seed | ||
) |
Sets the seed for the CRC.
This function sets the seed for the CRC to begin generating a signature with the given seed and all passed data. Using this function resets the CRC signature.
baseAddress | is the base address of the CRC module. |
seed | is the seed for the CRC to start generating a signature from. Modified bits are CRCINIRES of CRCINIRES register. |