7 #ifndef __MSP430WARE_CRC_H__
8 #define __MSP430WARE_CRC_H__
10 #include "inc/hw_memmap.h"
12 #ifdef __MSP430_HAS_CRC__
178 #endif // __MSP430WARE_CRC_H__
void CRC_set8BitData(uint16_t baseAddress, uint8_t dataIn)
Sets the 8 bit data to add into the CRC module to generate a new signature.
Definition: crc.c:33
uint16_t CRC_getResult(uint16_t baseAddress)
Returns the value pf the Signature Result.
Definition: crc.c:56
void CRC_set16BitDataReversed(uint16_t baseAddress, uint16_t dataIn)
Translates the 16 bit data by reversing the bits in each byte and then sets this data to add into the...
Definition: crc.c:39
void CRC_set16BitData(uint16_t baseAddress, uint16_t dataIn)
Sets the 16 bit data to add into the CRC module to generate a new signature.
Definition: crc.c:27
void CRC_set8BitDataReversed(uint16_t baseAddress, uint8_t dataIn)
Translates the 8 bit data by reversing the bits in each byte and then sets this data to add into the ...
Definition: crc.c:45
void CRC_setSeed(uint16_t baseAddress, uint16_t seed)
Sets the seed for the CRC.
Definition: crc.c:21
uint16_t CRC_getData(uint16_t baseAddress)
Returns the value currently in the Data register.
Definition: crc.c:51
uint16_t CRC_getResultBitsReversed(uint16_t baseAddress)
Returns the bit-wise reversed format of the Signature Result.
Definition: crc.c:61