Used in the Timer_B_initCaptureMode() function as the param parameter. More...
#include <timer_b.h>
Data Fields | |
uint16_t | captureRegister |
uint16_t | captureMode |
uint16_t | captureInputSelect |
uint16_t | synchronizeCaptureSource |
uint16_t | captureInterruptEnable |
uint16_t | captureOutputMode |
Used in the Timer_B_initCaptureMode() function as the param parameter.
uint16_t Timer_B_initCaptureModeParam::captureInputSelect |
Decides the Input Select
Valid values are:
Referenced by Timer_B_initCaptureMode().
uint16_t Timer_B_initCaptureModeParam::captureInterruptEnable |
Is to enable or disable Timer_B capture compare interrupt.
Valid values are:
Referenced by Timer_B_initCaptureMode().
uint16_t Timer_B_initCaptureModeParam::captureMode |
Is the capture mode selected.
Valid values are:
Referenced by Timer_B_initCaptureMode().
uint16_t Timer_B_initCaptureModeParam::captureOutputMode |
Specifies the output mode.
Valid values are:
Referenced by Timer_B_initCaptureMode().
uint16_t Timer_B_initCaptureModeParam::captureRegister |
Selects the capture register being used. Refer to datasheet to ensure the device has the capture register being used.
Valid values are:
Referenced by Timer_B_initCaptureMode().
uint16_t Timer_B_initCaptureModeParam::synchronizeCaptureSource |
Decides if capture source should be synchronized with Timer_B clock
Valid values are:
Referenced by Timer_B_initCaptureMode().