Used in the EUSCI_B_SPI_changeMasterClock() function as the param parameter. More...
#include <eusci_b_spi.h>
Data Fields | |
uint32_t | clockSourceFrequency |
Is the frequency of the selected clock source. | |
uint32_t | desiredSpiClock |
Is the desired clock rate for SPI communication. | |
Used in the EUSCI_B_SPI_changeMasterClock() function as the param parameter.