Used in the RTC_A_initCalendar() function as the CalendarTime parameter. More...
#include <rtc_a.h>
Data Fields | |
uint8_t | Seconds |
Seconds of minute between 0-59. | |
uint8_t | Minutes |
Minutes of hour between 0-59. | |
uint8_t | Hours |
Hour of day between 0-23. | |
uint8_t | DayOfWeek |
Day of week between 0-6. | |
uint8_t | DayOfMonth |
Day of month between 1-31. | |
uint8_t | Month |
Month between 0-11. | |
uint16_t | Year |
Year between 0-4095. | |
Used in the RTC_A_initCalendar() function as the CalendarTime parameter.
Used in the RTC_C_initCalendar() function as the CalendarTime parameter.
Used in the RTC_B_initCalendar() function as the CalendarTime parameter.