Data Fields
SysCtl_CSCalTLV_Info Struct Reference

#include <sysctl.h>

Data Fields

uint32_t rDCOIR_FCAL_RSEL04
 
uint32_t rDCOIR_FCAL_RSEL5
 
uint32_t rDCOIR_MAXPOSTUNE_RSEL04
 
uint32_t rDCOIR_MAXNEGTUNE_RSEL04
 
uint32_t rDCOIR_MAXPOSTUNE_RSEL5
 
uint32_t rDCOIR_MAXNEGTUNE_RSEL5
 
uint32_t rDCOIR_CONSTK_RSEL04
 
uint32_t rDCOIR_CONSTK_RSEL5
 
uint32_t rDCOER_FCAL_RSEL04
 
uint32_t rDCOER_FCAL_RSEL5
 
uint32_t rDCOER_MAXPOSTUNE_RSEL04
 
uint32_t rDCOER_MAXNEGTUNE_RSEL04
 
uint32_t rDCOER_MAXPOSTUNE_RSEL5
 
uint32_t rDCOER_MAXNEGTUNE_RSEL5
 
uint32_t rDCOER_CONSTK_RSEL04
 
uint32_t rDCOER_CONSTK_RSEL5
 

Field Documentation

uint32_t SysCtl_CSCalTLV_Info::rDCOIR_FCAL_RSEL04
uint32_t SysCtl_CSCalTLV_Info::rDCOIR_FCAL_RSEL5
uint32_t SysCtl_CSCalTLV_Info::rDCOIR_MAXPOSTUNE_RSEL04
uint32_t SysCtl_CSCalTLV_Info::rDCOIR_MAXNEGTUNE_RSEL04
uint32_t SysCtl_CSCalTLV_Info::rDCOIR_MAXPOSTUNE_RSEL5
uint32_t SysCtl_CSCalTLV_Info::rDCOIR_MAXNEGTUNE_RSEL5
uint32_t SysCtl_CSCalTLV_Info::rDCOIR_CONSTK_RSEL04
uint32_t SysCtl_CSCalTLV_Info::rDCOIR_CONSTK_RSEL5
uint32_t SysCtl_CSCalTLV_Info::rDCOER_FCAL_RSEL04
uint32_t SysCtl_CSCalTLV_Info::rDCOER_FCAL_RSEL5
uint32_t SysCtl_CSCalTLV_Info::rDCOER_MAXPOSTUNE_RSEL04
uint32_t SysCtl_CSCalTLV_Info::rDCOER_MAXNEGTUNE_RSEL04
uint32_t SysCtl_CSCalTLV_Info::rDCOER_MAXPOSTUNE_RSEL5
uint32_t SysCtl_CSCalTLV_Info::rDCOER_MAXNEGTUNE_RSEL5
uint32_t SysCtl_CSCalTLV_Info::rDCOER_CONSTK_RSEL04
uint32_t SysCtl_CSCalTLV_Info::rDCOER_CONSTK_RSEL5

The documentation for this struct was generated from the following file:

Copyright 2016, Texas Instruments Incorporated