Release Information
Click on the links in the table below to download.
|

|
What is MSP430Ware?
MSP430Ware is a collection of code
examples, datasheets and other
design resources for ALL MSP430 devices delivered in a convenient
package - essentially everything developers need to become MSP430
experts! Much like Stellaris MCU's StellarisWare and C2000 MCU's
ControlSUITE, MSP430Ware also includes high level peripheral driver
libraries to make it easy to talk to MSP430 hardware.
|
MSP430Ware Features:
- Collection of MSP430 design resources
- Sleek & intuitive GUI for browsing content
- Automatic filtering of content using a unique 2-pane
view
- Auto-updates through the web
- Features the MSP430 Driver Library
- Available as a CCS plugin or standalone executable
|
Learn more
about MSP430Ware and the Brand New Driver Library
MSP430Ware
@ a glance
MSP430 Driver Library, Delivered
through MSP430Ware
MSP430 Driver
Library is a simple API that
makes it easy to talk to your MSP430 5 series and 6 series devices.
Driver Library's abstracted API keeps you above the bits and bytes of
the MSP430 hardware by providing easy-to-use function calls. Thorough
documentation is delivered through a helpful API Guide, which includes
details on each function call and the recognized parameters. Developers
can use Driver Library functions to write complete projects with
minimal overhead!
Program unlike ever before with
MSP430 Driver Library
Download MSP430Ware
featuring Driver Library
Now!
How do I use MSP430Ware?
MSP430Ware is available as a
component of Code Composer Studio (CCS), or as a standalone package.
When delivered as a component of Code Composer Studio, the MSP430Ware
package can be navigated through a sleek GUI within the TI Resource
Explorer window in CCS.
- Recommended.
To get MSP430Ware and GUI-based front end, simply install the latest
version of Code Composer Studio version from the
table below
- Alternatively, MSP430Ware is available as a
standalone package.
However, this will only provide the folder structure of the MSP430Ware
package, and will not have a GUI-based front end. Download the
MSP430Ware executable in the table below.
- All FR57xx (IAR 5.40+) require CCS 5.3+.
- All FR5xx_6xx (IAR 5.51+) require CCS 5.4+.
Explaination of linker warnings on FR5xx devices?
Example Projects (both DriverLib and vanilla examples) for the
FR5xx families generate #10374-D
linker warnings due to a new feature in the CCS compiler. This
is
a benign warning and will be corrected in a future release.
See here
for an explanation of the warning.
How to Upgrade?
The easiest way to
upgrade is to start CCS and click Help->Install New
Software... This will find any new versions of MSP430ware and
optionally install them.
Another way to
upgrade is to download the MSP430ware_setup_xx_xx_xx_xx.exe and run it
after downloading.
Information for CCS 4.2.4 and IAR
5.20
Support
for CCS 4.2.4 and IAR 5.20 has been suspended with this release.
Please upgrade to a minimum CCS version of CCS 5.1.1 and IAR
5.40.
As in all previous MSP430ware releases Internet Explorer 7+ is needed
for Resource Explorer.
|
|
Legend
 |
Fill in Form. Approved users receive download URL in 1 minute. |
|
 |
Fill in Form. TI will contact you in 1-2+ business days. |
|