IEC60730 Class B API Documentation

Introduction

These software libraries allow for a variety of system tests required by IEC 60730-1:2010 for up to Class B products. The software libraries include projects that demonstrate running power-on self-test (POST) and periodic self-test (PST) with reporting conducted through flashing an LED. The user’s guide demonstrates how to integrate the POST and PST into an application design. In addition, the software package for IEC 60730 also includes a GUI configuration tool which allows users to easily generate customized configuration header files.

These APIs are broken out into the following sections:

Also note the existence of the following content available on disk. This is not part of this API but contains useful example code and documentation.


Copyright 2016, Texas Instruments Incorporated