Data Fields | |
| uint16_t | abortOnError |
| uint16_t | triggerSource |
| uint16_t | channelSelect |
| uint16_t | sideOfChannel |
| uint16_t | standByIndication |
| uint16_t | endOfSequence |
| uint16_t | earlyReceiveBias |
| uint16_t | enableChannelToggle |
| uint16_t SAPH_A_configASQParam::abortOnError |
Enables ASQ abort on errors if the conversion result is outside of expected value or an overflow/underflow condition occured.
Valid values are:
Referenced by SAPH_A_configureASQ().
| uint16_t SAPH_A_configASQParam::channelSelect |
Selects ASQ channel.
Valid values are:
Referenced by SAPH_A_configureASQ().
| uint16_t SAPH_A_configASQParam::earlyReceiveBias |
Selects early receive bias generating source.
Valid values are:
Referenced by SAPH_A_configureASQ().
| uint16_t SAPH_A_configASQParam::enableChannelToggle |
Enables channel toggle.
Valid values are:
Referenced by SAPH_A_configureASQ().
| uint16_t SAPH_A_configASQParam::endOfSequence |
Requests OFF in the end of sequence.
Valid values are:
Referenced by SAPH_A_configureASQ().
| uint16_t SAPH_A_configASQParam::sideOfChannel |
Selects pwn channel or opposite side channel to receive.
Valid values are:
Referenced by SAPH_A_configureASQ().
| uint16_t SAPH_A_configASQParam::standByIndication |
Selects standby indication.
Valid values are:
Referenced by SAPH_A_configureASQ().
| uint16_t SAPH_A_configASQParam::triggerSource |
Selects ASQ trigger source.
Valid values are:
Referenced by SAPH_A_configureASQ().