MSP430 USS Library 01_20_00_14
Release Notes
Document Revision: May 26, 2017
ADD MSP430 USS LIBRARY INTRODUCTION
This document is divided into the following sections:
01_20_00_14
What's New
- USS SW Library:
- Bug Fix:
- Renamed USS_HSPLL_Configuration member from ussXTALsettlelingCount to ussXTALsettlingCount
- Enhancement:
- Updated library to use default excitation bias of 0.4V nominal.
- Updated driverlib to version 2_91_00_20.
- Recompiled library and validated example projects with
SP_CCS_MSP430FR6047-Windows-2016-12-15T12-32
and SP_IAR_MSP430FR6047-Windows-2016-12-15T12-32.
- USS GUI demo project:
- Enhancement:
- Updated USS GUI example to Design Center based project.
- Enabled LCD functionality on EVM.
Revision History
01_20_00_13
- USS GUI demo project:
- Enhancement:
- Updated project to use USS_highFlow_option_version2 by default.
- Reduced USS_ALG_ABS_TOF_INTERVAL from 100 to 1
- USS SW Library:
- Enhancement:
- Added support for a second computation option for high flow (>5gpm) using absTOF measurements for cycle slip correction.
- Updated USS_Algorithms_User_Configuration structure. enableHighFlow bool flag in structure has been replace for enum highFlowOption. User can now select USS_highFlow_option_disabled, USS_highFlow_option_version1 or USS_highFlow_option_version2 via enum
- Updated template example project to use USS_highFlow_option_version2 by default
01_20_00_12
- USS GUI demo project:
- Enhancement:
- Updated project to use ussXTALsettlelingCount configuration parameter
- USS SW Library:
- Enhancement:
- Added support to specify USSXTAL settling time via a new parameter ussXTALsettlelingCount in USS_HSPLL_Configuration configuration structure.
- Added error code USS_message_code_HSPLL_invalid_settling_count_error. This error is returned if ussXTALsettlelingCount is set to 0.
- Updated template example project to use ussXTALsettlelingCount parameter
01_20_00_11
- USS GUI demo project:
- Bug Fix:
- Demo stopped sending ADC waveform after a reset.
- Enhancement:
- Check reset source and log fault if the source is unexpected (different from BOR or RST).
- Enabled Watchdog reset.
- USS SW Library:
- Bug Fix:
- UPS/DNS signals are lost if transducers are not connected the first time USS_runAlgorithms is called.
01_20_00_10
- Updated description for pulseLowPhasePeriod and pulseHighPhasePeriod.
- Updated description USS_runAlgorithmsFixedPoint, USS_runAlgorithms, and USS_startLowPowerUltrasonicCapture.
- Updated description USS_calibrateSignalGain API.
- Enabled accumulation and scaling of UPS/DNS captures. This functionality is enable via #define USS_SW_LIB_ENABLE_ACCUMULATION parameter in USS_userConfig.h
- Enabled resizing of LEA capture buffers using #define USS_SW_LIB_APP_MAX_CAPTURE_SIZE macro in USS_userConfig.h
- Updated library to define LEA RAM buffers outside of the library via USS configuration file. Current maximum UPS/DNS capture size is 620 without accumulation and 372 with accumulation enabled. Maximum capture size can be reduced to free up LEA memory.
- Fixed incorrect propagation delay configuraton.
- Renamed USS_Meter_Configuration *meterCofig; to USS_Meter_Configuration *meterConfig; in ussSwLib.h
- Added support for high flow rate
- Added the following members to Algorith Configuration structure:enableHighFlow, cycleSlipThreshold, thresholdX1X3
- Updated CCS linker command file to allow placing algorithm function in RAM. This is enabled by removing comments on #define __USS_RUN_ALG_FROM_RAM__ in lnk_msp430fr6047.cmd
01_20_00_09
- Updated description for pulseLowPhasePeriod and pulseHighPhasePeriod.
- Updated description USS_runAlgorithmsFixedPoint, USS_runAlgorithms, and USS_startLowPowerUltrasonicCapture.
- Updated description USS_calibrateSignalGain API.
- Enabled accumulation and scaling of UPS/DNS captures. This functionality is enable via #define USS_SW_LIB_ENABLE_ACCUMULATION parameter in USS_userConfig.h
- Enabled resizing of LEA capture buffers using #define USS_SW_LIB_APP_MAX_CAPTURE_SIZE macro in USS_userConfig.h
- Updated library to define LEA RAM buffers outside of the library via USS configuration file. Current maximum UPS/DNS capture size is 620 without accumulation and 372 with accumulation enabled. Maximum capture size can be reduced to free up LEA memory.
- Fixed incorrect propagation delay configuraton.
- Renamed USS_Meter_Configuration *meterCofig; to USS_Meter_Configuration *meterConfig; in ussSwLib.h
- Added support for high flow rate
- Added the following members to Algorith Configuration structure:enableHighFlow, cycleSlipThreshold, thresholdX1X3
- Updated CCS linker command file to allow placing algorithm function in RAM. This is enabled by removing comments on #define __USS_RUN_ALG_FROM_RAM__ in lnk_msp430fr6047.cmd
01_20_00_08
- Integrated optimized algortihms version 0_50_10_01
- Removed algorithn object from Library algorihtm object
- Updated USS_initAlgorithms to only require pointer to library configuration structure
- Increased capture buffer size from 400 to 500
- Removed elements from Algorithm configuration structure
- Added new APIS USS_getUPSPtr, USS_getDNSPtr, USS_setUPSPtr, USS_setDNSPtr
- Updated USS_initAlgorithms to force initialization of Algorithm object
- Updated documentation
- PEPTO results can be found ">here.
01_20_00_07
- Fixed JIRA bugs:
- Implemented USS_startLowPowerUltrasonicCapture API
- Evaluation of the non integer sampling freq and transducer freq fixed point implementation.
- Fixed minor bug impacting the first capture.
- Increased capture buffer size from 200 to 400.
- PEPTO results can be found here.
- Rebuild library using FR6047 SP v2016-10-26T12-43
01_10_08_03
- Fixed JIRA bugs:
- PEPTO results can be found here.
- Rebuild library using FR6047 SP v2016-10-26T12-43
1_10_05_03
- Fixed JIRA bugs:
- PEPTO results can be found here.
- Rebuild library using FR6047 SP v2016-10-13T10-02
1_10_03_00
PLL Output frequnecy configuration paramter is now configured as an enumeration
Refere to example configuration file to full list of User configuration file changes.
Fixed API name type "convertion" to "conversion"
Know issues IAR example project will throw a compilation error when invoking USS_runAlgorithms
USS Sw Library API UG documetation was updated.
1_10_00_00
- USS_calibrateGain
- USS_calculateDCOffset
- USS_startLowPowerUltrasonicCapture
1_00_00_05
- Updated doc/benchmarks/API_Benchmarks.docx file to match Power budget cycle count.
- Updated release notes to reflect support will be done via Bugzilla
Bug Fixes
1_00_00_04
Bug Fixes
New APIs
-
Added the following APIS (refer to Library API UG for implementation details):
- USS_message_code USS_calibrateIDAC(USS_SW_Library_configuration *config);
- USS_message_code USS_runAlgorithmsFixedPoint(USS_SW_Library_configuration *config,USS_Algorithms_Results_fixed_point *results);
- USS_message_code USS_updateABSTOFCalculationIteration(USS_SW_Library_configuration *config);
New structures
- Added new structure USS_Algorithms_Results_fixed_point. (refer to Library API UG for implementation details)
New enumeration elements
-
Added the following USS_message_code error codes (refer to API UG for more information):
-
USS_message_code_algorithm_error_invalid_iteration_value
-
USS_message_code_error_conversion_stopped_by_debugger
-
USS_message_code_algorithm_error_invalid_iteration_value
-
USS_message_code_Calibration_DAC_success
-
USS_message_code_Calibration_DAC_error
- Added USS_UUPS_Interrupt_STPBYDB enumeration field to USS_UUPS_Interrupt
New structure elements
-
Added the following elements to USS_Capture_Configuration structure (refer to Library API UG for implementation details):
- bool validMismatchDeltaValues;
- int8_t delta1;
- int8_t delta2;
-
Added new element to USS_Algorithms_User_Configuration structure (refer to Library API UG for implementation details):
- uint16_t absTOFIteration;
New Macro definitions
-
Added new bit USS_UUPS_STOPPED_BY_DEBUGGER to
USSSWLIB_USS_interrupt_status.
-
Global variable USSSWLIB_USS_interrupt_status
can be used to determine if UUPS STPBYDB interrupt was fired
during a USS capture.
Fixed typos
-
Fixed typos on USS_message_code enumeration:
-
USS_message_code_SAPH_update_error_ongoing_convertion to USS_message_code_SAPH_update_error_ongoing_conversion
-
USS_message_code_HSPLL_update_error_ongoing_convertion to USS_message_code_HSPLL_update_error_ongoing_conversion
-
USS_message_code_SDHS_update_error_ongoing_convertion to USS_message_code_SDHS_update_error_ongoing_conversion
-
USS_message_code_UUPS_update_error_ongoing_convertion to USS_message_code_UUPS_update_error_ongoing_conversion
0_80_00_02
This version of the library is a fully functional, not power optimized version
of USS SW Library.
0_00_00_06
The is a UNTESTED release of MSP430 USS SW Library.
Device Support
The following families of devices are support in this release of MSP430 USS
Library:
This
is the 01_20_00_14 release of MSP430 USS SW Library.
- CCS 6.1.0
- IAR 6.30.1
- IQ MAth libraries for MSP430FR5xx/6xx. This library is added as part of the
release. The template project is has has been setup to reference the library
included in this release.
This is an Enginnering release whith initial round of library
functional validation passed. In additon, intial system level validation for 4MHz
sampling frequency using Lab test data were performed.
Upgrade and Compatibility Information
The examples may be built with CCS.
Known Issues
None
This is build 01_20_00_14 of MSP430 USS SW library.
Bugs and enhancement request will be tracked via Bugzilla. To submit a bug
please use the following link Submit Bug or Enhancement request
Additional Resources
For more information, visit www.ti.com.