Used in the USCI_B_SPI_initMaster() function as the param parameter. More...
#include <usci_b_spi.h>
Data Fields | |
uint8_t | selectClockSource |
uint32_t | clockSourceFrequency |
Is the frequency of the selected clock source. | |
uint32_t | desiredSpiClock |
Is the desired clock rate for SPI communication. | |
uint8_t | msbFirst |
uint8_t | clockPhase |
uint8_t | clockPolarity |
Used in the USCI_B_SPI_initMaster() function as the param parameter.
uint8_t USCI_B_SPI_initMasterParam::clockPhase |
Is clock phase select.
Valid values are:
Referenced by USCI_B_SPI_initMaster().
uint8_t USCI_B_SPI_initMasterParam::clockPolarity |
Valid values are:
Referenced by USCI_B_SPI_initMaster().
uint8_t USCI_B_SPI_initMasterParam::msbFirst |
Controls the direction of the receive and transmit shift register.
Valid values are:
Referenced by USCI_B_SPI_initMaster().
uint8_t USCI_B_SPI_initMasterParam::selectClockSource |
Selects Clock source.
Valid values are:
Referenced by USCI_B_SPI_initMaster().