Used in the USCI_B_I2C_initMaster() function as the param parameter. More...
#include <usci_b_i2c.h>
Data Fields | |
uint8_t | selectClockSource |
uint32_t | i2cClk |
Is the rate of the clock supplied to the I2C module. | |
uint32_t | dataRate |
Used in the USCI_B_I2C_initMaster() function as the param parameter.
uint32_t USCI_B_I2C_initMasterParam::dataRate |
Set up for selecting data transfer rate.
Valid values are:
Referenced by USCI_B_I2C_initMaster().
uint8_t USCI_B_I2C_initMasterParam::selectClockSource |
Is the clocksource.
Valid values are:
Referenced by USCI_B_I2C_initMaster().