Used in the Timer_D_combineTDCCRToOutputPWM() function as the param parameter. More...
#include <timer_d.h>
Data Fields | |
uint16_t | clockSource |
uint16_t | clockSourceDivider |
uint16_t | clockingMode |
uint16_t | timerPeriod |
Is the specified timer period. | |
uint16_t | combineCCRRegistersCombination |
uint16_t | compareOutputMode |
uint16_t | dutyCycle1 |
Specifies the dutycycle for the generated waveform. | |
uint16_t | dutyCycle2 |
Specifies the dutycycle for the generated waveform. | |
Used in the Timer_D_combineTDCCRToOutputPWM() function as the param parameter.
uint16_t Timer_D_combineTDCCRToOutputPWMParam::clockingMode |
Is the selected clock mode register values.
Valid values are:
Referenced by Timer_D_combineTDCCRToOutputPWM().
uint16_t Timer_D_combineTDCCRToOutputPWMParam::clockSource |
Selects Clock source.
Valid values are:
Referenced by Timer_D_combineTDCCRToOutputPWM().
uint16_t Timer_D_combineTDCCRToOutputPWMParam::clockSourceDivider |
Is the divider for clock source.
Valid values are:
Referenced by Timer_D_combineTDCCRToOutputPWM().
uint16_t Timer_D_combineTDCCRToOutputPWMParam::combineCCRRegistersCombination |
Selects desired CCR registers to combine
Valid values are:
Referenced by Timer_D_combineTDCCRToOutputPWM().
uint16_t Timer_D_combineTDCCRToOutputPWMParam::compareOutputMode |
Specifies the output mode.
Valid values are:
Referenced by Timer_D_combineTDCCRToOutputPWM().