Data Fields
_EM_Phase_Results_ Struct Reference

Contains EM Phase Result. More...

#include <emSwLib.h>

Data Fields

uint32_t VRMS
 VRMS for previous frame (mV) More...
 
uint32_t IRMS
 IRMS for previous frame (uA) More...
 
uint32_t vPeak
 VPeak since system initialization (mV) More...
 
uint32_t iPeak
 IPeak since system initialization (uA) More...
 
int32_t powerFactor
 Power Factor calculated when the EM_powerFactor. More...
 
uint16_t frequency
 
EM_Power_t activePower
 Active Power for previous frame (uW) More...
 
EM_Power_t reactivePower
 Reactive Power for previous frame (uVAr) More...
 
EM_Power_t apparentPower
 Apparent Power for previous frame (uVA) More...
 
EM_Energy_t activeEnergy
 Active Energy for previous frame (uWh) More...
 
EM_Energy_t reactiveEnergy
 Reactive Energy for previous frame (uVArh) More...
 
EM_Energy_t apparentEnergy
 Apparent Energy for previous frame (uVAh) More...
 
EM_Phase phaseID
 Present Phase ID Name. More...
 

Detailed Description

Contains EM Phase Result.

Field Documentation

§ VRMS

uint32_t _EM_Phase_Results_::VRMS

VRMS for previous frame (mV)

§ IRMS

uint32_t _EM_Phase_Results_::IRMS

IRMS for previous frame (uA)

§ vPeak

uint32_t _EM_Phase_Results_::vPeak

VPeak since system initialization (mV)

§ iPeak

uint32_t _EM_Phase_Results_::iPeak

IPeak since system initialization (uA)

§ powerFactor

int32_t _EM_Phase_Results_::powerFactor

Power Factor calculated when the EM_powerFactor.

§ frequency

uint16_t _EM_Phase_Results_::frequency

The Frequency is stored in 0.01Hz steps. A 16 bit unsigned number supports the range 0.01Hz to 655.35Hz, which is clearly more than we will ever need for the fundamental.

§ activePower

EM_Power_t _EM_Phase_Results_::activePower

Active Power for previous frame (uW)

§ reactivePower

EM_Power_t _EM_Phase_Results_::reactivePower

Reactive Power for previous frame (uVAr)

§ apparentPower

EM_Power_t _EM_Phase_Results_::apparentPower

Apparent Power for previous frame (uVA)

§ activeEnergy

EM_Energy_t _EM_Phase_Results_::activeEnergy

Active Energy for previous frame (uWh)

§ reactiveEnergy

EM_Energy_t _EM_Phase_Results_::reactiveEnergy

Reactive Energy for previous frame (uVArh)

§ apparentEnergy

EM_Energy_t _EM_Phase_Results_::apparentEnergy

Apparent Energy for previous frame (uVAh)

§ phaseID

EM_Phase _EM_Phase_Results_::phaseID

Present Phase ID Name.


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale