Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
hal_adc_sd24.h File Reference

Detailed Description

Hardware Abstraction Layer for Sigma-Delta 24 (SD24)

Group: MSP Software Development

#include "sd24.h"
#include <stdint.h>
#include <stdbool.h>
Include dependency graph for hal_adc_sd24.h:

Go to the source code of this file.

Data Structures

struct  _HAL_ADC_SD24_Channel_
 Contains the SD24 Channel Configuration. More...
 
struct  _HAL_ADC_SD24_Configuration_
 Contains the SD24 Configuration. More...
 

Macros

#define HAL_ADC_CONV_INVALID_INDEX   0xFF
 Invalid Index for Converter Number. More...
 
#define HAL_ADC_MAX_MOD_FREQ   2097152L
 Maximum modulation frequency is 2MHz. More...
 
#define HAL_ADC_V_ARRAY_LENGTH   4
 Size of voltage array (it must be a multiple of 2) More...
 
#define HAL_ADC_I_ARRAY_LENGTH   4
 Size of voltage array (it must be a multiple of 2) More...
 
#define HAL_ADC_V_MASK   (HAL_ADC_V_ARRAY_LENGTH-1)
 Voltage Mask used for circular buffer. More...
 
#define HAL_ADC_I_MASK   (HAL_ADC_I_ARRAY_LENGTH-1)
 Current Mask used for circular buffer. More...
 
#define HAL_ADC_CH0_READ   (BIT0)
 
#define HAL_ADC_CH1_READ   (BIT1)
 
#define HAL_ADC_CH2_READ   (BIT2)
 
#define HAL_ADC_CH3_READ   (BIT3)
 
#define HAL_ADC_FREQ_4000_HZ   (4000)
 
#define HAL_ADC_FREQ_8000_HZ   (8000)
 
#define HAL_ADC_FREQ_16000_HZ   (16000)
 
#define HAL_ADC_PHASE_NO_DATA_READY   0x00
 
#define HAL_ADC_PHASE_A_DATA_READY   0x01
 
#define HAL_ADC_PHASE_B_DATA_READY   0x02
 
#define HAL_ADC_PHASE_C_DATA_READY   0x04
 
#define HAL_ADC_PHASE_NEUTRAL_DATA_READY   0x40
 
#define HAL_ADC_PHASE_TOTAL_DATA_READY   0x80
 
#define HAL_ADC_OSR_32   (32-1)
 
#define HAL_ADC_OSR_64   (64-1)
 
#define HAL_ADC_OSR_128   (128-1)
 
#define HAL_ADC_OSR_256   (256-1)
 

Typedefs

typedef enum _HAL_ADC_message_code_ HAL_ADC_message_code
 The following enumeration contain all possible HAL_ADC driver return message codes. More...
 
typedef struct _HAL_ADC_SD24_Channel_ HAL_ADC_SD24_Channel
 Contains the SD24 Channel Configuration. More...
 
typedef struct _HAL_ADC_SD24_Configuration_ HAL_ADC_SD24_Configuration
 Contains the SD24 Configuration. More...
 

Enumerations

enum  _HAL_ADC_message_code_ {
  HAL_ADC_message_code_no_error =0, HAL_ADC_message_code_invalid_freq_error =1, HAL_ADC_message_code_no_error =0, HAL_ADC_message_code_invalid_mod_freq_error =1,
  HAL_ADC_message_code_invalid_clock_divider_error =2
}
 The following enumeration contain all possible HAL_ADC driver return message codes. More...
 

Functions

HAL_ADC_message_code HAL_ADC_init (HAL_ADC_SD24_Configuration *config)
 The following API configures SD24 module based on user configuration files "emSwLib_userConfig.c" and "emSwLib_userConfig.h". More...
 
void HAL_ADC_startConversion (HAL_ADC_SD24_Configuration *config)
 The following API starts the enabled converters. More...
 
void HAL_ADC_stopConversion (HAL_ADC_SD24_Configuration *config)
 The following API stops the enabled converters. More...
 
void HAL_ADC_enableInterrupt (HAL_ADC_SD24_Configuration *config)
 The following API enables the interrupt for the master converter. More...
 
void HAL_ADC_disableInterrupt (HAL_ADC_SD24_Configuration *config)
 The following API disables the interrupt for the master converter. More...
 
void HAL_ADC_printResult (HAL_ADC_SD24_Configuration *config)
 The following API sends the stored results to the GUI. More...
 
void HAL_ADC_clearVariables (uint8_t phase)
 The following API clears all the global variables used in the ISR.) More...
 

Variables

volatile uint8_t phaseDataReady
 
HAL_ADC_SD24_Configuration halAdcConfig
 

Macro Definition Documentation

§ HAL_ADC_CONV_INVALID_INDEX

#define HAL_ADC_CONV_INVALID_INDEX   0xFF

Invalid Index for Converter Number.

(C) Copyright 2017, Texas Instruments, Inc.

§ HAL_ADC_MAX_MOD_FREQ

#define HAL_ADC_MAX_MOD_FREQ   2097152L

Maximum modulation frequency is 2MHz.

§ HAL_ADC_V_ARRAY_LENGTH

#define HAL_ADC_V_ARRAY_LENGTH   4

Size of voltage array (it must be a multiple of 2)

§ HAL_ADC_I_ARRAY_LENGTH

#define HAL_ADC_I_ARRAY_LENGTH   4

Size of voltage array (it must be a multiple of 2)

§ HAL_ADC_V_MASK

#define HAL_ADC_V_MASK   (HAL_ADC_V_ARRAY_LENGTH-1)

Voltage Mask used for circular buffer.

§ HAL_ADC_I_MASK

#define HAL_ADC_I_MASK   (HAL_ADC_I_ARRAY_LENGTH-1)

Current Mask used for circular buffer.

§ HAL_ADC_CH0_READ

#define HAL_ADC_CH0_READ   (BIT0)

§ HAL_ADC_CH1_READ

#define HAL_ADC_CH1_READ   (BIT1)

§ HAL_ADC_CH2_READ

#define HAL_ADC_CH2_READ   (BIT2)

§ HAL_ADC_CH3_READ

#define HAL_ADC_CH3_READ   (BIT3)

§ HAL_ADC_FREQ_4000_HZ

#define HAL_ADC_FREQ_4000_HZ   (4000)

§ HAL_ADC_FREQ_8000_HZ

#define HAL_ADC_FREQ_8000_HZ   (8000)

§ HAL_ADC_FREQ_16000_HZ

#define HAL_ADC_FREQ_16000_HZ   (16000)

§ HAL_ADC_PHASE_NO_DATA_READY

#define HAL_ADC_PHASE_NO_DATA_READY   0x00

§ HAL_ADC_PHASE_A_DATA_READY

#define HAL_ADC_PHASE_A_DATA_READY   0x01

§ HAL_ADC_PHASE_B_DATA_READY

#define HAL_ADC_PHASE_B_DATA_READY   0x02

§ HAL_ADC_PHASE_C_DATA_READY

#define HAL_ADC_PHASE_C_DATA_READY   0x04

§ HAL_ADC_PHASE_NEUTRAL_DATA_READY

#define HAL_ADC_PHASE_NEUTRAL_DATA_READY   0x40

§ HAL_ADC_PHASE_TOTAL_DATA_READY

#define HAL_ADC_PHASE_TOTAL_DATA_READY   0x80

§ HAL_ADC_OSR_32

#define HAL_ADC_OSR_32   (32-1)

§ HAL_ADC_OSR_64

#define HAL_ADC_OSR_64   (64-1)

§ HAL_ADC_OSR_128

#define HAL_ADC_OSR_128   (128-1)

§ HAL_ADC_OSR_256

#define HAL_ADC_OSR_256   (256-1)

Typedef Documentation

§ HAL_ADC_message_code

The following enumeration contain all possible HAL_ADC driver return message codes.

§ HAL_ADC_SD24_Channel

Contains the SD24 Channel Configuration.

§ HAL_ADC_SD24_Configuration

Contains the SD24 Configuration.

Enumeration Type Documentation

§ _HAL_ADC_message_code_

The following enumeration contain all possible HAL_ADC driver return message codes.

Enumerator
HAL_ADC_message_code_no_error 

This message code is returned when no error was detected while invoking the API.

HAL_ADC_message_code_invalid_freq_error 

This message code is returned when the input frequency is not supported.

HAL_ADC_message_code_no_error 

This message code is returned when no error was detected while invoking the API.

HAL_ADC_message_code_invalid_mod_freq_error 

This message code is returned when the modulation frequency (OSR*sampFreq) is greater than 2Mhz

HAL_ADC_message_code_invalid_clock_divider_error 

This message code is returned when the clock divider multiplier (SMCLK / (OSR * sampleFreq) is not supported.

© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale