Logo
MSP DSP Library
matrix_ex1_add_q15.c

This example demonstrates how to use the msp_matrix_add_q15 API to perform addition of two real source matrices.

//******************************************************************************
// Add two real 16-bit matrices.
//
// Brent Peterson, Jeremy Friesenhahn
// Texas Instruments Inc.
// April 2016
//******************************************************************************
#include "msp430.h"
#include <math.h>
#include <stdint.h>
#include <stdbool.h>
#include "DSPLib.h"
/* Input signal parameters */
#define FS 8192
#define SIGNAL_ROWS 10
#define SIGNAL_COLS 12
#define SIGNAL_FREQUENCY1 200
#define SIGNAL_AMPLITUDE1 0.6
#define SIGNAL_FREQUENCY2 2100
#define SIGNAL_AMPLITUDE2 0.15
/* Constants */
#define PI 3.1415926536
/* Input matrix A */
DSPLIB_DATA(inputA,4)
_q15 inputA[SIGNAL_ROWS][SIGNAL_COLS];
/* Input matrix B */
DSPLIB_DATA(inputB,4)
_q15 inputB[SIGNAL_ROWS][SIGNAL_COLS];
/* Result of the matrix add */
DSPLIB_DATA(result,4)
_q15 result[SIGNAL_ROWS][SIGNAL_COLS];
/* Benchmark cycle counts */
volatile uint32_t cycleCount;
/* Function prototypes */
extern void initSignals(void);
void main(void)
{
msp_status status;
/* Disable WDT. */
WDTCTL = WDTPW + WDTHOLD;
#ifdef __MSP430_HAS_PMM__
/* Disable GPIO power-on default high-impedance mode for FRAM devices */
PM5CTL0 &= ~LOCKLPM5;
#endif
/* Initialize input signals */
initSignals();
/* Initialize the parameter structure. */
addParams.rows = SIGNAL_ROWS;
addParams.cols = SIGNAL_COLS;
/* Invoke the msp_matrix_add_q15 API. */
msp_benchmarkStart(MSP_BENCHMARK_BASE, 1);
status = msp_matrix_add_q15(&addParams, *inputA, *inputB, *result);
cycleCount = msp_benchmarkStop(MSP_BENCHMARK_BASE);
msp_checkStatus(status);
/* End of program. */
__no_operation();
}
void initSignals(void)
{
uint16_t i;
msp_status status;
/*
* Generate a set of linearly increasing in frequency sine waves for each
* row of matrices in Q15 format.
*/
for (i = 0; i < SIGNAL_ROWS; i++) {
/* Generate Q15 input signal 1 */
sinParams.length = SIGNAL_COLS;
sinParams.amplitude = _Q15(SIGNAL_AMPLITUDE1);
sinParams.cosOmega = _Q15(cosf((float)i*2*PI*SIGNAL_FREQUENCY1/FS/(float)SIGNAL_ROWS));
sinParams.sinOmega = _Q15(sinf((float)i*2*PI*SIGNAL_FREQUENCY1/FS/(float)SIGNAL_ROWS));
status = msp_sinusoid_q15(&sinParams, inputA[i]);
msp_checkStatus(status);
/* Generate Q15 input signal 2 */
sinParams.length = SIGNAL_COLS;
sinParams.amplitude = _Q15(SIGNAL_AMPLITUDE2);
sinParams.cosOmega = _Q15(cosf((float)i*2*PI*SIGNAL_FREQUENCY2/FS/(float)SIGNAL_ROWS));
sinParams.sinOmega = _Q15(sinf((float)i*2*PI*SIGNAL_FREQUENCY2/FS/(float)SIGNAL_ROWS));
status = msp_sinusoid_q15(&sinParams, inputB[i]);
msp_checkStatus(status);
}
}