MSP430™CapTIvateSoftwareLibraryAPIGuide
1_83_00_05
|
#include <CAPT_Protocol.h>
Data Fields | |
int8_t | i8currPacketIndex |
bool | bStuffedByteDetected |
typedef tTLProtocolProcessingVariables holds "static" variables that the protocol layer uses during packet framing. These variables are used by the CAPT_processReceivedData API.
int8_t tTLProtocolProcessingVariables::i8currPacketIndex |
bool tTLProtocolProcessingVariables::bStuffedByteDetected |