MSP430™CapTIvateSoftwareLibraryAPIGuide
1_83_00_05
|
#include <CAPT_Type.h>
Data Fields | |
IQ16_t | SliderPosition |
Current slider/wheel position stored as a filtered value. More... | |
uint16_t | ui16Resolution |
Specifies the slider/wheel resolution in points. More... | |
uint16_t | SliderLower |
Lower slider trim/stretch point (not applicable to wheels) More... | |
uint16_t | SliderUpper |
Upper slider trim/stretch point (not applicable to wheels) More... | |
uint8_t | SliderBeta |
Specifies the beta coefficient of the slider/wheel position filter. More... | |
uint8_t | ui8TotalElements |
Total elements in slider/wheel sensor (pre-populated) More... | |
tPositionAlgorithm | SliderAlgorithm: 4 |
Position algorithm type (16 possible options) More... | |
bool | SliderFilterEnable: 1 |
Slider/wheel position filter enable. More... | |
bool | Reseed: 1 |
Flag the slider/wheel position filter for an immediate reseed. More... | |
typedef tSliderSensorParams
Slider/Wheel sensor specific parameters. One instance must be created and tied to every slider or wheel sensor.
IQ16_t tSliderSensorParams::SliderPosition |
Current slider/wheel position stored as a filtered value.
uint16_t tSliderSensorParams::ui16Resolution |
Specifies the slider/wheel resolution in points.
uint16_t tSliderSensorParams::SliderLower |
Lower slider trim/stretch point (not applicable to wheels)
uint16_t tSliderSensorParams::SliderUpper |
Upper slider trim/stretch point (not applicable to wheels)
uint8_t tSliderSensorParams::SliderBeta |
Specifies the beta coefficient of the slider/wheel position filter.
uint8_t tSliderSensorParams::ui8TotalElements |
Total elements in slider/wheel sensor (pre-populated)
tPositionAlgorithm tSliderSensorParams::SliderAlgorithm |
Position algorithm type (16 possible options)
bool tSliderSensorParams::SliderFilterEnable |
Slider/wheel position filter enable.
bool tSliderSensorParams::Reseed |
Flag the slider/wheel position filter for an immediate reseed.