MSP430™CapTIvateSoftwareLibraryAPIGuide
1_83_00_05
|
#include <CAPT_Type.h>
Data Fields | |
tSensor ** | pSensor |
uint8_t | ui8NumberOfSensors |
typedef tProxSensorParams
Proximity sensor specific parameters. One instance must be created and tied to every proximity sensor.
tSensor** tProxSensorParams::pSensor |
Pointer to an array of sensor pointers that should be activated as Tx electrodes during the proximity measurement (if in projected capacitance mode).
uint8_t tProxSensorParams::ui8NumberOfSensors |
Indicates how many sensors are activated as Tx electrodes during the proximity measurement (if in projected capacitance mode).