MSP430™CapTIvateSoftwareLibraryAPIGuide  1_83_00_05
Data Fields
tGenericSensorParams Struct Reference

#include <CAPT_Type.h>

Data Fields

uint16_t ui16Value
 Generic Value. More...
 
uint16_t ui16Parameter
 Generic Parameter. More...
 

Detailed Description

typedef tGenericSensorParams

Place holder for pointer to sensor specific parameters. Sensor-specific structures are tied in to the sensor stucture by casting the sensor parameter structure to a generic sensor parameters structure.

Field Documentation

§ ui16Value

uint16_t tGenericSensorParams::ui16Value

Generic Value.

§ ui16Parameter

uint16_t tGenericSensorParams::ui16Parameter

Generic Parameter.


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale