|
tTLParameterAccessResult | CAPT_accessTrackPadSensorParameter (tSensor **sensorArray, tParameterPacket *pPacket) |
| Access a special CapTIvate™ TL structure variable for a TrackPad sensor. More...
|
|
uint16_t | CAPT_getCyclePacket (tSensor **sensorArray, uint8_t ui8SensorID, uint8_t ui8Cycle, uint8_t *pBuffer) |
|
uint16_t | CAPT_getSensorPacket (tSensor **sensorArray, uint8_t ui8SensorID, uint8_t *pBuffer) |
|
uint16_t | CAPT_getGeneralPurposePacket (uint16_t *pData, uint8_t ui8Cnt, uint8_t *pBuffer) |
|
uint16_t | CAPT_getStringPacket (const char *pSrcString, uint8_t *pBuffer) |
|
uint16_t | CAPT_getTrackPadPacket (tSensor **sensorArray, uint8_t ui8SensorID, uint8_t *pBuffer) |
|
uint16_t | CAPT_getTrackPadSensorStatusPacket (tSensor **sensorArray, uint8_t ui8SensorID, uint8_t *pBuffer) |
|
uint16_t | CAPT_getChecksum (const uint8_t *pBuffer, const uint16_t ui16Length) |
| This API calculate the checksum of a byte buffer of given length. More...
|
|
bool | CAPT_verifyChecksum (const uint8_t *pBuffer, const uint16_t ui16Length, const uint16_t ui16Checksum) |
| This API verifies the checksum of a byte buffer of given length. More...
|
|
uint16_t | CAPT_stuffSyncBytes (uint8_t *pBuffer, uint16_t ui16Length) |
|
bool | CAPT_processReceivedData (tByteQueue *pReceiveQueue, tParameterPacket *pPacket, tTLProtocolProcessingVariables *pVariables) |
|
tTLParameterAccessResult | CAPT_accessSensorParameter (tSensor **sensorArray, tParameterPacket *pPacket) |
|
tTLParameterAccessResult | CAPT_accessSpecialSensorParameter (tSensor **sensorArray, tParameterPacket *pPacket) |
|