MSP430™CapTIvateSoftwareLibraryAPIGuide
1_83_00_05
|
#include <CAPT_Type.h>
Data Fields | |
uint16_t | ui16Value |
Generic Value. More... | |
uint16_t | ui16Parameter |
Generic Parameter. More... | |
typedef tGenericSensorParams
Place holder for pointer to sensor specific parameters. Sensor-specific structures are tied in to the sensor stucture by casting the sensor parameter structure to a generic sensor parameters structure.
uint16_t tGenericSensorParams::ui16Value |
Generic Value.
uint16_t tGenericSensorParams::ui16Parameter |
Generic Parameter.