MSP430™CapTIvateSoftwareLibraryAPIGuide
1_83_00_05
|
typedef tDeBounceSettings More...
#include <CAPT_Type.h>
Data Fields | |
uint8_t | DbIn: 4 |
uint8_t | DbOut: 4 |
typedef tDeBounceSettings
The de-bounce structure holds de-bounce up/down information, and can be used for storing de-bounce thresholds or counts.
uint8_t tDeBounceSettings::DbIn |
De-bounce into a Touch/Prox State May hold the threshold or the current de-bounce count
uint8_t tDeBounceSettings::DbOut |
De-bounce out of a Touch/Prox State May hold the threshold or the current de-bounce count