|
| file | _atoIQN.c |
| | Functions to convert a string to an IQN number.
|
| |
| file | _IQNasin_acos.c |
| | Functions to compute the inverse sine of the input and return the result, in radians.
|
| |
| file | _IQNatan2.c |
| | Functions to compute the 4-quadrant arctangent of the input and return the result.
|
| |
| file | _IQNdiv.c |
| | Functions to divide two values of IQN type.
|
| |
| file | _IQNexp.c |
| | Functions to compute the exponential of the input and return the result.
|
| |
| file | _IQNfrac.c |
| | Functions to return the fractional portion of the input.
|
| |
| file | _IQNlog.c |
| | Functions to compute the base-e logarithm of an IQN number.
|
| |
| file | _IQNmpy.c |
| | Functions to multiply two values of IQN type.
|
| |
| file | _IQNmpyIQX.c |
| | Functions to multiply two IQ numbers in different IQ formats, returning the product in a third IQ format. The result is neither rounded nor saturated, so if the product is greater than the minimum or maximum values for the given output IQ format, the return value will wrap around and produce inaccurate results.
|
| |
| file | _IQNrmpy.c |
| | Functions to multiply two IQ numbers, returning the product in IQ format. The result is rounded but not saturated, so if the product is greater than the minimum or maximum values for the given IQ format, the return value wraps around and produces inaccurate results.
|
| |
| file | _IQNrsmpy.c |
| | Functions to multiply two IQ numbers, returning the product in IQ format. The result is rounded and saturated, so if the product is greater than the minimum or maximum values for the given IQ format, the return value is saturated to the minimum or maximum value for the given IQ format (as appropriate).
|
| |
| file | _IQNsin_cos.c |
| | Functions to compute the sine and cosine of the input and return the result.
|
| |
| file | _IQNsqrt.c |
| | Functions to compute square root, inverse square root and the magnitude of two IQN inputs.
|
| |
| file | _IQNtoa.c |
| | Functions to convert an IQ number to a string.
|
| |
| file | _IQNtoF.c |
| | Functions to convert IQN type to floating point.
|
| |