![]() |
![]() |
|
MSPM0L111X Driver Library
2.10.00.04
|
|
Modules | |
| DL_GPIO_PIN | |
| DL_GPIO_EDGE_POLARITY | |
| DL_GPIO_INPUT_FILTER | |
Functions | |
| __STATIC_INLINE void | DL_GPIO_enablePower (GPIO_Regs *gpio) |
| Enables the Peripheral Write Enable (PWREN) register for the GPIO. More... | |
| __STATIC_INLINE void | DL_GPIO_disablePower (GPIO_Regs *gpio) |
| Disables the Peripheral Write Enable (PWREN) register for the GPIO. More... | |
| __STATIC_INLINE bool | DL_GPIO_isPowerEnabled (GPIO_Regs *gpio) |
| Returns if the Peripheral Write Enable (PWREN) register for the GPIO is enabled. More... | |
| __STATIC_INLINE void | DL_GPIO_reset (GPIO_Regs *gpio) |
| Resets gpio peripheral. More... | |
| __STATIC_INLINE bool | DL_GPIO_isReset (GPIO_Regs *gpio) |
| Returns if gpio peripheral was reset. More... | |
| __STATIC_INLINE void | DL_GPIO_initDigitalOutput (uint32_t pincmIndex) |
| Configures a pin as a basic GPIO output. More... | |
| __STATIC_INLINE void | DL_GPIO_initDigitalOutputFeatures (uint32_t pincmIndex, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_DRIVE_STRENGTH driveStrength, DL_GPIO_HIZ hiZ) |
| Configures a pin as a GPIO output. More... | |
| __STATIC_INLINE void | DL_GPIO_setDigitalInternalResistor (uint32_t pincmIndex, DL_GPIO_RESISTOR internalResistor) |
| Configures internal resistor for digital pin. More... | |
| __STATIC_INLINE void | DL_GPIO_setAnalogInternalResistor (uint32_t pincmIndex, DL_GPIO_RESISTOR internalResistor) |
| Configures internal resistor for analog pin. More... | |
| __STATIC_INLINE void | DL_GPIO_initDigitalInput (uint32_t pincmIndex) |
| Configures a pin as a basic GPIO input. More... | |
| __STATIC_INLINE void | DL_GPIO_initDigitalInputFeatures (uint32_t pincmIndex, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_HYSTERESIS hysteresis, DL_GPIO_WAKEUP wakeup) |
| Configures a pin as a GPIO input. More... | |
| __STATIC_INLINE void | DL_GPIO_initPeripheralFunction (uint32_t pincmIndex, uint32_t function) |
| Configure a pin to operate with peripheral functionality. More... | |
| __STATIC_INLINE void | DL_GPIO_initPeripheralOutputFunction (uint32_t pincmIndex, uint32_t function) |
| Configure a pin to operate with peripheral output functionality. More... | |
| __STATIC_INLINE void | DL_GPIO_initPeripheralOutputFunctionFeatures (uint32_t pincmIndex, uint32_t function, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_DRIVE_STRENGTH driveStrength, DL_GPIO_HIZ hiZ) |
| Configure a pin to operate with peripheral output functionality with optional features. More... | |
| __STATIC_INLINE void | DL_GPIO_initPeripheralInputFunction (uint32_t pincmIndex, uint32_t function) |
| Configure a pin to operate with peripheral input functionality. More... | |
| __STATIC_INLINE void | DL_GPIO_initPeripheralInputFunctionFeatures (uint32_t pincmIndex, uint32_t function, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_HYSTERESIS hysteresis, DL_GPIO_WAKEUP wakeup) |
| Configure a pin to operate with peripheral input functionality with optional features. More... | |
| __STATIC_INLINE void | DL_GPIO_initPeripheralAnalogFunction (uint32_t pincmIndex) |
| Configure a pin to operate with analog functionality. More... | |
| __STATIC_INLINE void | DL_GPIO_enableWakeUp (uint32_t pincmIndex) |
| Set GPIO pin's wakeup enable bit. More... | |
| __STATIC_INLINE void | DL_GPIO_disableWakeUp (uint32_t pincmIndex) |
| Clear GPIO pin's wakeup enable bit. More... | |
| __STATIC_INLINE bool | DL_GPIO_isWakeUpEnabled (uint32_t pincmIndex) |
| Returns if GPIO pin's wake up bit is enabled. More... | |
| __STATIC_INLINE void | DL_GPIO_setWakeupCompareValue (uint32_t pincmIndex, DL_GPIO_WAKEUP_COMPARE_VALUE value) |
| Set the compare value to use for wake for the specified pin. More... | |
| __STATIC_INLINE DL_GPIO_WAKEUP_COMPARE_VALUE | DL_GPIO_getWakeupCompareValue (uint32_t pincmIndex) |
| Get the compare value to use for wake for the specified pin. More... | |
| __STATIC_INLINE bool | DL_GPIO_isWakeStateGenerated (uint32_t pincmIndex) |
| Checks if the GPIO pin's Wake State bit is active. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_readPins (GPIO_Regs *gpio, uint32_t pins) |
| Read a group of GPIO pins. More... | |
| __STATIC_INLINE void | DL_GPIO_writePins (GPIO_Regs *gpio, uint32_t pins) |
| Write a group of GPIO pins. More... | |
| __STATIC_INLINE void | DL_GPIO_writePinsVal (GPIO_Regs *gpio, uint32_t pinsMask, uint32_t pinsVal) |
| Update the value of one or more GPIO pins. More... | |
| __STATIC_INLINE void | DL_GPIO_setPins (GPIO_Regs *gpio, uint32_t pins) |
| Set a group of GPIO pins. More... | |
| __STATIC_INLINE void | DL_GPIO_clearPins (GPIO_Regs *gpio, uint32_t pins) |
| Clear a group of GPIO pins. More... | |
| __STATIC_INLINE void | DL_GPIO_togglePins (GPIO_Regs *gpio, uint32_t pins) |
| Toggle a group of GPIO pins. More... | |
| __STATIC_INLINE void | DL_GPIO_enableOutput (GPIO_Regs *gpio, uint32_t pins) |
| Enable output on a group of GPIO pins. More... | |
| __STATIC_INLINE void | DL_GPIO_disableOutput (GPIO_Regs *gpio, uint32_t pins) |
| Disable output on a group of GPIO pins. More... | |
| __STATIC_INLINE void | DL_GPIO_enableDMAAccess (GPIO_Regs *gpio, uint32_t pins) |
| Enable DMA access on a group of pins. More... | |
| __STATIC_INLINE void | DL_GPIO_disableDMAAccess (GPIO_Regs *gpio, uint32_t pins) |
| Disable DMA access on a group of pins. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_isDMAccessEnabled (GPIO_Regs *gpio, uint32_t pins) |
| Check if DMA access is enabled on a group of pins. More... | |
| __STATIC_INLINE void | DL_GPIO_setLowerPinsPolarity (GPIO_Regs *gpio, uint32_t polarity) |
| Set the polarity of all bits [0, 15] in the group of pins. More... | |
| __STATIC_INLINE void | DL_GPIO_setUpperPinsPolarity (GPIO_Regs *gpio, uint32_t polarity) |
| Set the polarity of all bits [16, 31] in the group of pins. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_getLowerPinsPolarity (GPIO_Regs *gpio) |
| Get the polarity of bits [0, 15] in the group of pins. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_getUpperPinsPolarity (GPIO_Regs *gpio) |
| Get the polarity of bits [16, 31] in the group of pins. More... | |
| __STATIC_INLINE void | DL_GPIO_setLowerPinsInputFilter (GPIO_Regs *gpio, uint32_t filter) |
| Set the input filter of bits [0, 15] in the group of pins. More... | |
| __STATIC_INLINE void | DL_GPIO_setUpperPinsInputFilter (GPIO_Regs *gpio, uint32_t filter) |
| Set the input filter of bits [16, 31] in the group of pins. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_getLowerPinsInputFilter (GPIO_Regs *gpio) |
| Get the input filter of bits [0, 15] in the group of pins. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_getUpperPinsInputFilter (GPIO_Regs *gpio) |
| Get the input filter of bits [16, 31] in the group of pins. More... | |
| __STATIC_INLINE void | DL_GPIO_enableGlobalFastWake (GPIO_Regs *gpio) |
| Enable Global Fast Wake. More... | |
| __STATIC_INLINE void | DL_GPIO_disableGlobalFastWake (GPIO_Regs *gpio) |
| Disable Global Fast Wake. More... | |
| __STATIC_INLINE void | DL_GPIO_enableFastWakePins (GPIO_Regs *gpio, uint32_t pins) |
| Enable fast wake for pins. More... | |
| __STATIC_INLINE void | DL_GPIO_disableFastWakePins (GPIO_Regs *gpio, uint32_t pins) |
| Disable fast wake for pins. More... | |
| __STATIC_INLINE void | DL_GPIO_enableHiZ (uint32_t pincmIndex) |
| Enable Hi-Z for the pin. More... | |
| __STATIC_INLINE void | DL_GPIO_disableHiZ (uint32_t pincmIndex) |
| Disable Hi-Z for the pin. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_getEnabledFastWakePins (GPIO_Regs *gpio, uint32_t pins) |
| Check which pins have fast wake feature enabled. More... | |
| __STATIC_INLINE void | DL_GPIO_enableInterrupt (GPIO_Regs *gpio, uint32_t pins) |
| Enable GPIO interrupts. More... | |
| __STATIC_INLINE void | DL_GPIO_disableInterrupt (GPIO_Regs *gpio, uint32_t pins) |
| Disable GPIO interrupts. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_getEnabledInterrupts (GPIO_Regs *gpio, uint32_t pins) |
| Check which GPIO interrupts are enabled. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_getEnabledInterruptStatus (GPIO_Regs *gpio, uint32_t pins) |
| Check interrupt flag of enabled GPIO interrupts. More... | |
| __STATIC_INLINE void | DL_GPIO_setInterrupt (GPIO_Regs *gpio, uint32_t pins) |
| Set interrupt flag of any GPIO. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_getRawInterruptStatus (GPIO_Regs *gpio, uint32_t pins) |
| Check interrupt flag of any GPIO interrupt. More... | |
| __STATIC_INLINE DL_GPIO_IIDX | DL_GPIO_getPendingInterrupt (GPIO_Regs *gpio) |
| Get highest priority pending GPIO interrupt. More... | |
| __STATIC_INLINE void | DL_GPIO_clearInterruptStatus (GPIO_Regs *gpio, uint32_t pins) |
| Clear pending GPIO interrupts. More... | |
| __STATIC_INLINE void | DL_GPIO_configSubscriber (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index, DL_GPIO_SUBSCRIBER_OUT_POLICY policy, DL_GPIO_SUBSCRIBERx_PIN pinIndex) |
| Configures GPIO subscriber. This API preserves enable/disbale status of subscriber. More... | |
| __STATIC_INLINE void | DL_GPIO_enableSubscriber (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index) |
| Enables GPIO subscriber. More... | |
| __STATIC_INLINE void | DL_GPIO_disableSubscriber (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index) |
| Disables GPIO subscriber. More... | |
| __STATIC_INLINE bool | DL_GPIO_isSubscriberEnabled (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index) |
| Returns if GPIO subscriber is enabled. More... | |
| __STATIC_INLINE void | DL_GPIO_setPublisherChanID (GPIO_Regs *gpio, DL_GPIO_PUBLISHER_INDEX index, uint8_t chanID) |
| Sets the event publisher channel id. More... | |
| __STATIC_INLINE uint8_t | DL_GPIO_getPublisherChanID (GPIO_Regs *gpio, DL_GPIO_PUBLISHER_INDEX index) |
| Gets the event publisher channel id. More... | |
| __STATIC_INLINE void | DL_GPIO_setSubscriberChanID (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index, uint8_t chanID) |
| Sets the event subscriber channel id. More... | |
| __STATIC_INLINE uint8_t | DL_GPIO_getSubscriberChanID (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index) |
| Gets the event subscriber channel id. More... | |
| __STATIC_INLINE void | DL_GPIO_enableEvents (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins) |
| Enables GPIO events. More... | |
| __STATIC_INLINE void | DL_GPIO_disableEvents (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins) |
| Disable GPIO events. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_getEnabledEvents (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins) |
| Check which GPIO events are enabled. More... | |
| __STATIC_INLINE uint32_t | DL_GPIO_getEnabledEventStatus (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins) |
| Checks if any of the GPIO events which were previously enabled are pending. More... | |
| __STATIC_INLINE void | DL_GPIO_clearEventStatus (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins) |
| Clear pending GPIO event. More... | |
The GPIO Driver Library allows full configuration of the MSPM0 GPIO module. The GPIO peripheral provides the user with a means to write data out and read data in to and from the device pins. It also provides a way to detect wakeup events while the device is in a low power state.
| enum DL_GPIO_INVERSION |
| enum DL_GPIO_RESISTOR |
| enum DL_GPIO_HYSTERESIS |
| enum DL_GPIO_WAKEUP |
| enum DL_GPIO_HIZ |
| enum DL_GPIO_EVENT_ROUTE |
| enum DL_GPIO_IIDX |
| __STATIC_INLINE void DL_GPIO_enablePower | ( | GPIO_Regs * | gpio | ) |
Enables the Peripheral Write Enable (PWREN) register for the GPIO.
Before any peripheral registers can be configured by software, the peripheral itself must be enabled by writing the ENABLE bit together with the appropriate KEY value to the peripheral's PWREN register.
| gpio | Pointer to the register overlay for the peripheral |
| __STATIC_INLINE void DL_GPIO_disablePower | ( | GPIO_Regs * | gpio | ) |
Disables the Peripheral Write Enable (PWREN) register for the GPIO.
When the PWREN.ENABLE bit is cleared, the peripheral's registers are not accessible for read/write operations.
| gpio | Pointer to the register overlay for the peripheral |
| __STATIC_INLINE bool DL_GPIO_isPowerEnabled | ( | GPIO_Regs * | gpio | ) |
Returns if the Peripheral Write Enable (PWREN) register for the GPIO is enabled.
Before any peripheral registers can be configured by software, the peripheral itself must be enabled by writing the ENABLE bit together with the appropriate KEY value to the peripheral's PWREN register.
When the PWREN.ENABLE bit is cleared, the peripheral's registers are not accessible for read/write operations.
| gpio | Pointer to the register overlay for the peripheral |
| __STATIC_INLINE void DL_GPIO_reset | ( | GPIO_Regs * | gpio | ) |
Resets gpio peripheral.
| gpio | Pointer to the register overlay for the peripheral |
| __STATIC_INLINE bool DL_GPIO_isReset | ( | GPIO_Regs * | gpio | ) |
Returns if gpio peripheral was reset.
| gpio | Pointer to the register overlay for the peripheral |
| __STATIC_INLINE void DL_GPIO_initDigitalOutput | ( | uint32_t | pincmIndex | ) |
Configures a pin as a basic GPIO output.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| __STATIC_INLINE void DL_GPIO_initDigitalOutputFeatures | ( | uint32_t | pincmIndex, |
| DL_GPIO_INVERSION | inversion, | ||
| DL_GPIO_RESISTOR | internalResistor, | ||
| DL_GPIO_DRIVE_STRENGTH | driveStrength, | ||
| DL_GPIO_HIZ | hiZ | ||
| ) |
Configures a pin as a GPIO output.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| [in] | inversion | Enable Inversion of the pin output. One of DL_GPIO_INVERSION. |
| [in] | internalResistor | Internal resistor to use. One of DL_GPIO_RESISTOR. |
| [in] | driveStrength | Enable High-Drive for the pin. One of DL_GPIO_DRIVE_STRENGTH. |
| [in] | hiZ | Enable/disable Hi-Z for the pin. One of DL_GPIO_HIZ. |
| __STATIC_INLINE void DL_GPIO_setDigitalInternalResistor | ( | uint32_t | pincmIndex, |
| DL_GPIO_RESISTOR | internalResistor | ||
| ) |
Configures internal resistor for digital pin.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| [in] | internalResistor | Internal resistor to use. One of DL_GPIO_RESISTOR. |
References DL_GPIO_RESISTOR_PULL_DOWN, and DL_GPIO_RESISTOR_PULL_UP.
| __STATIC_INLINE void DL_GPIO_setAnalogInternalResistor | ( | uint32_t | pincmIndex, |
| DL_GPIO_RESISTOR | internalResistor | ||
| ) |
Configures internal resistor for analog pin.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| [in] | internalResistor | Internal resistor to use. One of DL_GPIO_RESISTOR. |
| __STATIC_INLINE void DL_GPIO_initDigitalInput | ( | uint32_t | pincmIndex | ) |
Configures a pin as a basic GPIO input.
Configures the pin as a basic GPIO input. If you want to use additional features of the input mode, refer to DL_GPIO_initDigitalInputFeatures.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| __STATIC_INLINE void DL_GPIO_initDigitalInputFeatures | ( | uint32_t | pincmIndex, |
| DL_GPIO_INVERSION | inversion, | ||
| DL_GPIO_RESISTOR | internalResistor, | ||
| DL_GPIO_HYSTERESIS | hysteresis, | ||
| DL_GPIO_WAKEUP | wakeup | ||
| ) |
Configures a pin as a GPIO input.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| [in] | inversion | Enable Inversion of the pin input. One of DL_GPIO_INVERSION. |
| [in] | internalResistor | Internal resistor to use. One of DL_GPIO_RESISTOR. |
| [in] | hysteresis | Enable/disable Hysteresis on the pin. One of DL_GPIO_HYSTERESIS. |
| [in] | wakeup | Configure wakeup behavior for the pin. One of DL_GPIO_WAKEUP. |
| __STATIC_INLINE void DL_GPIO_initPeripheralFunction | ( | uint32_t | pincmIndex, |
| uint32_t | function | ||
| ) |
Configure a pin to operate with peripheral functionality.
| [in] | pincmIndex | The PINCM register index that maps to the target pin to configure the peripheral functionality for |
| [in] | function | Function to configure the pin for. See definition of IOMUX_PINCMx_PF_xxx in the device header file. |
| __STATIC_INLINE void DL_GPIO_initPeripheralOutputFunction | ( | uint32_t | pincmIndex, |
| uint32_t | function | ||
| ) |
Configure a pin to operate with peripheral output functionality.
| [in] | pincmIndex | The PINCM register index that maps to the target pin to configure the peripheral functionality for |
| [in] | function | Function to configure the pin for. See definition of IOMUX_PINCMx_PF_xxx in the device header file. |
| __STATIC_INLINE void DL_GPIO_initPeripheralOutputFunctionFeatures | ( | uint32_t | pincmIndex, |
| uint32_t | function, | ||
| DL_GPIO_INVERSION | inversion, | ||
| DL_GPIO_RESISTOR | internalResistor, | ||
| DL_GPIO_DRIVE_STRENGTH | driveStrength, | ||
| DL_GPIO_HIZ | hiZ | ||
| ) |
Configure a pin to operate with peripheral output functionality with optional features.
| [in] | pincmIndex | The PINCM register index that maps to the target pin to configure the peripheral functionality for |
| [in] | function | Function to configure the pin for. Check definition of IOMUX_PINCMx_PF_xxx in the device header file. |
| [in] | inversion | Enable Inversion of the pin output. One of DL_GPIO_INVERSION. |
| [in] | internalResistor | Internal resistor to use. One of DL_GPIO_RESISTOR. |
| [in] | driveStrength | Enable High-Drive for the pin. One of DL_GPIO_DRIVE_STRENGTH. |
| [in] | hiZ | Enable/disable Hi-Z for the pin. One of DL_GPIO_HIZ. |
| __STATIC_INLINE void DL_GPIO_initPeripheralInputFunction | ( | uint32_t | pincmIndex, |
| uint32_t | function | ||
| ) |
Configure a pin to operate with peripheral input functionality.
| [in] | pincmIndex | The PINCM register index that maps to the target pin to configure the peripheral functionality for |
| [in] | function | Function to configure the pin for. See definition of IOMUX_PINCMx_PF_xxx in the device header file. |
| __STATIC_INLINE void DL_GPIO_initPeripheralInputFunctionFeatures | ( | uint32_t | pincmIndex, |
| uint32_t | function, | ||
| DL_GPIO_INVERSION | inversion, | ||
| DL_GPIO_RESISTOR | internalResistor, | ||
| DL_GPIO_HYSTERESIS | hysteresis, | ||
| DL_GPIO_WAKEUP | wakeup | ||
| ) |
Configure a pin to operate with peripheral input functionality with optional features.
| [in] | pincmIndex | The PINCM register index that maps to the target pin to configure the peripheral functionality for |
| [in] | function | Function to configure the pin for. See definition of IOMUX_PINCMx_PF_xxx in the device header file. |
| [in] | inversion | Enable Inversion of the pin input. One of DL_GPIO_INVERSION. |
| [in] | internalResistor | Internal resistor to use. One of DL_GPIO_RESISTOR. |
| [in] | hysteresis | Enable/disable Hystersis on the pin. One of DL_GPIO_HYSTERESIS. |
| [in] | wakeup | Configure wakeup behavior for the pin. One of DL_GPIO_WAKEUP. |
| __STATIC_INLINE void DL_GPIO_initPeripheralAnalogFunction | ( | uint32_t | pincmIndex | ) |
Configure a pin to operate with analog functionality.
| [in] | pincmIndex | The PINCM register index that maps to the target pin to configure the analog functionality for |
| __STATIC_INLINE void DL_GPIO_enableWakeUp | ( | uint32_t | pincmIndex | ) |
Set GPIO pin's wakeup enable bit.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
References DL_GPIO_WAKEUP_ENABLE.
| __STATIC_INLINE void DL_GPIO_disableWakeUp | ( | uint32_t | pincmIndex | ) |
Clear GPIO pin's wakeup enable bit.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| __STATIC_INLINE bool DL_GPIO_isWakeUpEnabled | ( | uint32_t | pincmIndex | ) |
Returns if GPIO pin's wake up bit is enabled.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| __STATIC_INLINE void DL_GPIO_setWakeupCompareValue | ( | uint32_t | pincmIndex, |
| DL_GPIO_WAKEUP_COMPARE_VALUE | value | ||
| ) |
Set the compare value to use for wake for the specified pin.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| [in] | value | The wakeup compare value to set. One of DL_GPIO_WAKEUP_COMPARE_VALUE |
References DL_Common_updateReg().
| __STATIC_INLINE DL_GPIO_WAKEUP_COMPARE_VALUE DL_GPIO_getWakeupCompareValue | ( | uint32_t | pincmIndex | ) |
Get the compare value to use for wake for the specified pin.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| One | of DL_GPIO_WAKEUP_COMPARE_VALUE |
| __STATIC_INLINE bool DL_GPIO_isWakeStateGenerated | ( | uint32_t | pincmIndex | ) |
Checks if the GPIO pin's Wake State bit is active.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin. |
| __STATIC_INLINE uint32_t DL_GPIO_readPins | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Read a group of GPIO pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Pins to read. Bitwise OR of DL_GPIO_PIN. |
| Bitwise | OR of DL_GPIO_PIN of pins that are currently high from the input selection. |
| __STATIC_INLINE void DL_GPIO_writePins | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Write a group of GPIO pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Pins to write. All enabled GPIO pins will be set to the equivalent bit value in pins. |
| __STATIC_INLINE void DL_GPIO_writePinsVal | ( | GPIO_Regs * | gpio, |
| uint32_t | pinsMask, | ||
| uint32_t | pinsVal | ||
| ) |
Update the value of one or more GPIO pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pinsMask | The GPIO pin(s) you want to update. Bitwise OR of DL_GPIO_PIN. |
| [in] | pinsVal | Value(s) for the GPIO pin(s) you want to update. Only the values for pins specified in pinsMask will change. |
| __STATIC_INLINE void DL_GPIO_setPins | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Set a group of GPIO pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Pins to set high. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE void DL_GPIO_clearPins | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Clear a group of GPIO pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Pins to clear. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE void DL_GPIO_togglePins | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Toggle a group of GPIO pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Pins to toggle. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE void DL_GPIO_enableOutput | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Enable output on a group of GPIO pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Pins to enable output. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE void DL_GPIO_disableOutput | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Disable output on a group of GPIO pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Pins to disable output. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE void DL_GPIO_enableDMAAccess | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Enable DMA access on a group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Pins to toggle. Bitwise OR of DL_GPIO_PIN. |
References DL_Common_updateReg().
| __STATIC_INLINE void DL_GPIO_disableDMAAccess | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Disable DMA access on a group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Pins to disable DMA access on. Bitwise OR of DL_GPIO_PIN. |
References DL_Common_updateReg().
| __STATIC_INLINE uint32_t DL_GPIO_isDMAccessEnabled | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Check if DMA access is enabled on a group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Pins to check DMA access on. Bitwise OR of DL_GPIO_PIN. |
| Bitwise | OR of DL_GPIO_PIN values |
| __STATIC_INLINE void DL_GPIO_setLowerPinsPolarity | ( | GPIO_Regs * | gpio, |
| uint32_t | polarity | ||
| ) |
Set the polarity of all bits [0, 15] in the group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | polarity | Bitwise OR of DL_GPIO_EDGE_POLARITY for pins [0, 15] |
| __STATIC_INLINE void DL_GPIO_setUpperPinsPolarity | ( | GPIO_Regs * | gpio, |
| uint32_t | polarity | ||
| ) |
Set the polarity of all bits [16, 31] in the group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | polarity | Bitwise OR of DL_GPIO_EDGE_POLARITY for pins [16, 31] |
| __STATIC_INLINE uint32_t DL_GPIO_getLowerPinsPolarity | ( | GPIO_Regs * | gpio | ) |
Get the polarity of bits [0, 15] in the group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| Polarity | setting with bitwise OR of DL_GPIO_EDGE_POLARITY for pins [0, 15] |
| __STATIC_INLINE uint32_t DL_GPIO_getUpperPinsPolarity | ( | GPIO_Regs * | gpio | ) |
Get the polarity of bits [16, 31] in the group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| Polarity | setting with bitwise OR of DL_GPIO_EDGE_POLARITY for pins [16, 31] |
| __STATIC_INLINE void DL_GPIO_setLowerPinsInputFilter | ( | GPIO_Regs * | gpio, |
| uint32_t | filter | ||
| ) |
Set the input filter of bits [0, 15] in the group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | filter | Bitwise OR of DL_GPIO_INPUT_FILTER for pins [0, 15] |
| __STATIC_INLINE void DL_GPIO_setUpperPinsInputFilter | ( | GPIO_Regs * | gpio, |
| uint32_t | filter | ||
| ) |
Set the input filter of bits [16, 31] in the group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | filter | Bitwise OR of DL_GPIO_INPUT_FILTER for pins [16, 31] |
| __STATIC_INLINE uint32_t DL_GPIO_getLowerPinsInputFilter | ( | GPIO_Regs * | gpio | ) |
Get the input filter of bits [0, 15] in the group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| Input | filter setting with bitwise OR of DL_GPIO_INPUT_FILTER for pins [0, 15] |
| __STATIC_INLINE uint32_t DL_GPIO_getUpperPinsInputFilter | ( | GPIO_Regs * | gpio | ) |
Get the input filter of bits [16, 31] in the group of pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| Input | filter setting with bitwise OR of DL_GPIO_INPUT_FILTER for pins [16, 31] |
| __STATIC_INLINE void DL_GPIO_enableGlobalFastWake | ( | GPIO_Regs * | gpio | ) |
Enable Global Fast Wake.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| __STATIC_INLINE void DL_GPIO_disableGlobalFastWake | ( | GPIO_Regs * | gpio | ) |
Disable Global Fast Wake.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| __STATIC_INLINE void DL_GPIO_enableFastWakePins | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Enable fast wake for pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Bit mask of pins to enable fast-wake feature. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE void DL_GPIO_disableFastWakePins | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Disable fast wake for pins.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Bit mask of pins to disable fast-wake feature. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE void DL_GPIO_enableHiZ | ( | uint32_t | pincmIndex | ) |
Enable Hi-Z for the pin.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin |
| __STATIC_INLINE void DL_GPIO_disableHiZ | ( | uint32_t | pincmIndex | ) |
Disable Hi-Z for the pin.
| [in] | pincmIndex | The PINCM register index that maps to the target GPIO pin |
| __STATIC_INLINE uint32_t DL_GPIO_getEnabledFastWakePins | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Check which pins have fast wake feature enabled.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Bit mask of pins to check. Bitwise OR of DL_GPIO_PIN. |
| Bitwise | OR of DL_GPIO_PIN values |
| __STATIC_INLINE void DL_GPIO_enableInterrupt | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Enable GPIO interrupts.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Bit mask of interrupts to enable. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE void DL_GPIO_disableInterrupt | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Disable GPIO interrupts.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Bit mask of interrupts to disable. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE uint32_t DL_GPIO_getEnabledInterrupts | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Check which GPIO interrupts are enabled.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Bit mask of interrupts to check. Bitwise OR of DL_GPIO_PIN. |
| Bitwise | OR of DL_GPIO_PIN values |
| __STATIC_INLINE uint32_t DL_GPIO_getEnabledInterruptStatus | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Check interrupt flag of enabled GPIO interrupts.
Checks if any of the GPIO interrupts that were previously enabled are pending.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Bit mask of interrupts to check. Bitwise OR of DL_GPIO_PIN. |
| Bitwise | OR of DL_GPIO_PIN values |
| __STATIC_INLINE void DL_GPIO_setInterrupt | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Set interrupt flag of any GPIO.
Manually set a GPIO interrupt to be pending
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Bit mask of interrupts to set. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE uint32_t DL_GPIO_getRawInterruptStatus | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Check interrupt flag of any GPIO interrupt.
Checks if any of the GPIO interrupts are pending. Interrupts do not have to be previously enabled.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Bit mask of interrupts to check. Bitwise OR of DL_GPIO_PIN. |
| Bitwise | OR of DL_GPIO_PIN values |
| __STATIC_INLINE DL_GPIO_IIDX DL_GPIO_getPendingInterrupt | ( | GPIO_Regs * | gpio | ) |
Get highest priority pending GPIO interrupt.
Checks if any of the GPIO interrupts are pending. Interrupts do not have to be previously enabled.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| One | of DL_GPIO_IIDX |
| __STATIC_INLINE void DL_GPIO_clearInterruptStatus | ( | GPIO_Regs * | gpio, |
| uint32_t | pins | ||
| ) |
Clear pending GPIO interrupts.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | pins | Bit mask of interrupts to check. Bitwise OR of DL_GPIO_PIN. |
| __STATIC_INLINE void DL_GPIO_configSubscriber | ( | GPIO_Regs * | gpio, |
| DL_GPIO_SUBSCRIBER_INDEX | index, | ||
| DL_GPIO_SUBSCRIBER_OUT_POLICY | policy, | ||
| DL_GPIO_SUBSCRIBERx_PIN | pinIndex | ||
| ) |
Configures GPIO subscriber. This API preserves enable/disbale status of subscriber.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the subscriber event index to be configured |
| [in] | policy | Specifies the the GPIO behavior when the subscriber receives publisher event. |
| [in] | pinIndex | Specifies the GPIO bit number which will be targeted by the subscriber action. |
References DL_Common_updateReg().
| __STATIC_INLINE void DL_GPIO_enableSubscriber | ( | GPIO_Regs * | gpio, |
| DL_GPIO_SUBSCRIBER_INDEX | index | ||
| ) |
Enables GPIO subscriber.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the subscriber event index to be configured |
| __STATIC_INLINE void DL_GPIO_disableSubscriber | ( | GPIO_Regs * | gpio, |
| DL_GPIO_SUBSCRIBER_INDEX | index | ||
| ) |
Disables GPIO subscriber.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the subscriber event index to be configured |
| __STATIC_INLINE bool DL_GPIO_isSubscriberEnabled | ( | GPIO_Regs * | gpio, |
| DL_GPIO_SUBSCRIBER_INDEX | index | ||
| ) |
Returns if GPIO subscriber is enabled.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the subscriber event index to be configured |
| __STATIC_INLINE void DL_GPIO_setPublisherChanID | ( | GPIO_Regs * | gpio, |
| DL_GPIO_PUBLISHER_INDEX | index, | ||
| uint8_t | chanID | ||
| ) |
Sets the event publisher channel id.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the register event index to be configured |
| [in] | chanID | Channel ID number. Valid range 0-15. If ChanID == 0 subscriber is disconnected. Consult your device datasheet on the actual maximum number of channels. |
| __STATIC_INLINE uint8_t DL_GPIO_getPublisherChanID | ( | GPIO_Regs * | gpio, |
| DL_GPIO_PUBLISHER_INDEX | index | ||
| ) |
Gets the event publisher channel id.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the register event index to be configured |
| __STATIC_INLINE void DL_GPIO_setSubscriberChanID | ( | GPIO_Regs * | gpio, |
| DL_GPIO_SUBSCRIBER_INDEX | index, | ||
| uint8_t | chanID | ||
| ) |
Sets the event subscriber channel id.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the register event index to be configured |
| [in] | chanID | Channel ID number. Valid range 0-15. If ChanID == 0 subscriber is disconnected. Consult your device datasheet on the actual maximum number of channels. |
| __STATIC_INLINE uint8_t DL_GPIO_getSubscriberChanID | ( | GPIO_Regs * | gpio, |
| DL_GPIO_SUBSCRIBER_INDEX | index | ||
| ) |
Gets the event subscriber channel id.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the register event index to be configured |
| __STATIC_INLINE void DL_GPIO_enableEvents | ( | GPIO_Regs * | gpio, |
| DL_GPIO_EVENT_ROUTE | index, | ||
| uint32_t | pins | ||
| ) |
Enables GPIO events.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the register event index to be configured |
| [in] | pins | Valid options will depend on index argument. When index == DL_GPIO_EVENT_ROUTE_1, valid pins values are bitwise OR of DL_GPIO_PIN (0-15). When index == DL_GPIO_EVENT_ROUTE_2, valid pins Bitwise OR of DL_GPIO_PIN (16-31). |
References DL_GPIO_EVENT_ROUTE_1, and DL_GPIO_EVENT_ROUTE_2.
| __STATIC_INLINE void DL_GPIO_disableEvents | ( | GPIO_Regs * | gpio, |
| DL_GPIO_EVENT_ROUTE | index, | ||
| uint32_t | pins | ||
| ) |
Disable GPIO events.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the register event index to be configured |
| [in] | pins | Valid options will depend on index argument. When index == DL_GPIO_EVENT_ROUTE_1, valid pins values are bitwise OR of DL_GPIO_PIN (0-15). When index == DL_GPIO_EVENT_ROUTE_2, valid pins Bitwise OR of DL_GPIO_PIN (16-31). |
References DL_GPIO_EVENT_ROUTE_1, and DL_GPIO_EVENT_ROUTE_2.
| __STATIC_INLINE uint32_t DL_GPIO_getEnabledEvents | ( | GPIO_Regs * | gpio, |
| DL_GPIO_EVENT_ROUTE | index, | ||
| uint32_t | pins | ||
| ) |
Check which GPIO events are enabled.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the register event index to be configured |
| [in] | pins | Valid options will depend on index argument. When index == DL_GPIO_EVENT_ROUTE_1, valid pins values are bitwise OR of DL_GPIO_PIN (0-15). When index == DL_GPIO_EVENT_ROUTE_2, valid pins Bitwise OR of DL_GPIO_PIN (16-31). |
| Bitwise | OR of DL_GPIO_PIN values |
| __STATIC_INLINE uint32_t DL_GPIO_getEnabledEventStatus | ( | GPIO_Regs * | gpio, |
| DL_GPIO_EVENT_ROUTE | index, | ||
| uint32_t | pins | ||
| ) |
Checks if any of the GPIO events which were previously enabled are pending.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the register event index to be configured |
| [in] | pins | Valid options will depend on index argument. When index == DL_GPIO_EVENT_ROUTE_1, valid pins values are bitwise OR of DL_GPIO_PIN (0-15). When index == DL_GPIO_EVENT_ROUTE_2, valid pins Bitwise OR of DL_GPIO_PIN (16-31). |
| Bitwise | OR of DL_GPIO_PIN values |
| __STATIC_INLINE void DL_GPIO_clearEventStatus | ( | GPIO_Regs * | gpio, |
| DL_GPIO_EVENT_ROUTE | index, | ||
| uint32_t | pins | ||
| ) |
Clear pending GPIO event.
| [in] | gpio | Pointer to the register overlay for the peripheral |
| [in] | index | Specifies the register event index to be configured |
| [in] | pins | Valid options will depend on index argument. When index == DL_GPIO_EVENT_ROUTE_1, valid pins values are bitwise OR of DL_GPIO_PIN (0-15). When index == DL_GPIO_EVENT_ROUTE_2, valid pins Bitwise OR of DL_GPIO_PIN (16-31). |
References DL_GPIO_EVENT_ROUTE_1, and DL_GPIO_EVENT_ROUTE_2.