MSPM0 Universal FOC Software User’s Guide

1. CCS Project setup

  1. Go to Import CCS Projects as shown below.

  2. Click Browse. Navigate to C:\ti\mspm0_sdk_<SDK_Version>\examples\nortos\[LAUNCHPAD]\motor_control_universal_foc.

  3. Click Select Folder. Check the desired hardware board, and click Finish to import the project into your workspace.

Register Overview

The Universal FOC Library is structured to be interfaced through Specific Registers, the Registers will be periodically parsed by the application interface to convert to the FOC algorithm variables. This helps users to have a clear interface to the motor control software.

For using the FOC library the user need to use the 3 main registers namely UserCtrlRegs, UserInputRegs and UserStatusRegs. The Library exposes these registers through pointers.

The pointers for 3 registers:

  • pUserCtrlRegs

    All the variables used for controlling the motor like speed input is present in this user controls structure

  • pUserInputRegs

    All the configurations like different startup modes etc are present in the User input registers

  • pUserStatusRegs

    Used for monitoring the algorithm status and algorithm variables

Configuring the Project

For running the motor we first need to configure the userInputRegs with the correct parameters.

There are 2 types of parameters present in the userInputRegs:

  • System parameters

    This sets the motor parameters, and hardware defined parameters like Current base value, Voltage base value .etc. The system parameters are present in pUserInputRegs→systemParams.

  • Tuning parameters

    All the other elements in the userInputRegs except systemParams are the tuning parameters. The tuning parameter helps to tune the motor to the desired performance. for example in mtrStartUp1 we can configure the startup methods like align, slow first start and IPD. Refer to the Tuning Document for more details.

The FOC library initializes the input registers to a default value it is present in the setUserDefaultMotorParameters() function in ISR.c file. The default motor parameters are for LVSERVOMTR motor available at ti.com .

Refer to the Tuning Document for details on configurations.

Starting the Project

  1. Connect the hardware and turn on the power supply. There should be no more than 50mA on the power supply.

  2. Click on the Build button.image0 Project should build with no errors.

  3. Click on the Debug button. image1

  4. Open the Expressions window and add the following global structures pointers.

  • pUserCtrlRegs

  • pUserInputRegs

  • pUserStatusRegs

  1. Press Play image2 to start the code.

  2. Enable “Continuous Refresh” in the Expressions window. image3

  3. Refer to the Tuning Document for spinning and tuning the motor.

2. Register Map

1 UserCtrlRegs

Set of registers used to control the motor.

1.1 SpeedCtrl

Speed control register

SpeedCtrl

Definition

speedInput

Speed Command in 15 bit value. Value to set = (Desired motor speed) x 32768/(Max motor speed)

1.2 algoDebugCtrl1

Algorithm debug register 1

algoDebugCtrl1

Definition

forceAlignAngleSrcSelect

Force align angle state source select

forceISDEn

Halts after ISD is complete

forceIPDEn

Halts after IPD is complete

forceSlowCycleFirstCycleEn

Halts after slow first cycle is complete

forceAlignEn

Halts after align is complete

closeLoopDis

Disable open to closed loop transition

forcedAlignAngle

Align angle used in forced align

clearFlt

Clears all faults

1.3 algoDebugCtrl2

Algorithm debug register 2

algoDebugCtrl2

Definition

forceVQCurrLoopDis

Vq applied when current loop and speed loop are disabled

forceVDCurrLoopDis

Vd applied when current loop and speed loop are disabled

currLoopDis

Disable current loop and speed loop

statusUpdateEn

Enables continous update of the UserStatusRegs

updateConfigs

If set 1, firmware will set to zero when all the motor control configurations updated

updateSysParams

If set 1, firmware will periodically update system paramters

NOTE: If user updates all or many of the configurations in pUserInputRegs, to ensure that the parameters are updated by the motor control application to the FOC variables user should make the updateConfigs as 1 and wait till it is set 0 by the firmware before giving any speed input. This done to ensure all the parameters set by the user gets updated to the FOC variables.

1.4 algoDebugCtrl3

Algorithm debug register 3

algoDebugCtrl3

Definition

fluxModeReference

Id reference used when Flux Mode is Enabled

1.5 dacCtrl

DAC control register

dacCtrl

Definition

dacEn

DAC enable

dacShift

Unipolar ouput Left or right shift, used if dacScalingFactor is 0

dacScalingFactor

Dac scale factor in iq 27

dacOutAddr

Variable address to output through DAC

NOTE: Even if dacEn is set to 1 the output will not be seen in the DAC pin if DAC peripheral is not enabled, DAC peripheral need to be set enabled in TI Sysconfig for DAC peripheral to function. User has to take care the DAC pin is not used while enabling the DAC peripheral in TI SysConfig

2 UserInputRegs

Registers for user input parameters

2.1 System Parameters

Configuration for system parameters

System Parameters

Definition

mtrResist

Motor Phase resistance in milli Ω (ohms)

mtrInductance

Motor Phase Inductance in Micro Henry

mtrSaliency

Motor inductance saliency percentage

mtrBemfConst

Motor BEMF Constant in milli Volts Per Hertz

voltageBase

Maximum Board Supply voltage in Volts = (voltage division scaling ratio x 3.3v)

currentBase

Maximum Current measurable by the board = (3.3v/(2 x CSA_GAIN x SENSE_RESISTOR))

maxMotorSpeed

Rated Speed of the Motor/ Maximum operational Speed

speedLoopKp

Proportional Gain for Closed Loop Speed Control

speedLoopKi

Integral Gain for Closed Loop Speed Control

currLoopKp

Proportional Gain for Closed Loop Torque Control

currLoopKi

Integral Gain for Closed Loop Torque Control

fluxWeakeningKi

Integral Controller Gain for Flux Weakening

fluxWeakeningKp

Proportional Control Gain for Flux Weakening

kSlide

Kslide for esmo

2.2 isdCfg

Configuration Parameters for Initial Speed Detection

isdCfg

Bit Wise Definition

statDetectThr

BEMF threshold to detect if motor is stationary

hiZTime

Motor Coasting time when Coasting is Enabled during Initial Speed Synchronization

brkTime

Motor Braking time when Braking is Enabled during Initial Speed Synchronization

brkConfig

Brake configuration for time based or current based braking

fwDrvResyncThr

Minimum speed threshold to resynchronize to close loop (% of

MAX_SPEED)

resyncEn

Enable Resynchronization of Motor when motor is already spinning during startup

rvsDrEn

Enable Resynchronization of Motor and reverse the direction when motor is already spinning in reverse direction during startup

hiZEn

Enable Coasting of Motor when motor is already spinning during startup with higher speeds before Resynchronization

brakeEn

Enable Braking of Motor when motor is already spinning during startup with higher speeds before Resynchronization

isdEn

ISD enable

2.3 mtrStartUp1

Configuration Parameters for Motor Start up methods

mtrStartUp1

Bit Wise Definition

olILimitCfg

Open loop current reference configuration

ipdRepeat

Number of times IPD is executed to average the estimated resultant rotor position

ipdAdvAngle

Motor Startup angle advancement from IPD detected rotor angle for maximizing torque output

ipdCurrThresh

IPD current threshold

ipdClkFreq

IPD Clock Frequency

alignOrSlowCurrLimit

Align or slow first cycle current limit

alignTime

Time in mS for aligning the rotor during Motor startup

alignSlowRampRate

Align, slow first cycle and open loop current ramp rate

mtrStartUpOption

Motor startup selection from Align/ IPD /Slow First Cycle after Initial Speed Detection

2.4 mtrStartUp2

Configuration Parameters for Motor Start up methods

mtrStartUp2

Bit Wise Definition

thetaErrRampRate

Ramp rate for reducing difference between estimated theta and open loop theta while transitioning to closed loop

FirstCycFreqSel

First cycle frequency in open loop for align, double align and IPDn

slowFirstCycFreq

Frequency of first cycle in close loop startup (% of MAX_SPEED)

alignAngle

Motor Start up Align Angle

olClHandOffThr

Open to close loop handoff threshold (% of MAX_SPEED)

olAcc2

2nd Order Open Loop Speed Ramp up

olAcc1

1st Order Open Loop Speed Ramp up

olILimit

Current Limit reference during Open Loop Acceleration

2.5 closeLoop1

Configuration Parameters for Closed Loop Speed/Torque Mode

closeLoop1

Bit Wise Definition

avsEn

Enable limiting sudden Rise in DC bus (Anti Voltage Surge) during Faster Motor decelerations

pwmMode

Enable/Disable Continous SVM modulation

pwmFreqOut

Set the Switching PWM Frequency (Max : 75KHZ)

clDec

Closed loop Speed/torque reference Ramp down setting

clDecCfg

Configuration selection for Cldec between ClAcc/ClDec

clAcc

Closed loop Speed/torque reference Ramp up settingp

overModEnable

Enable Over Modulation (non sinusoidal modulation over the modulation Index)

mtrStopOption

Motor Stop Option to choose from Hi-z / Active Spin Down

iLimit

Maximum current reference in torque PI loop

highFreqFOCEn

Reduces the ADC sampling rate to half value, so that PWM freq can be high

2.6 closeLoop2

Configuration Parameters for Closed Loop Speed/Torque Mode

closeLoop2

Bit Wise Definition

leadAngle

Lead angle for voltage control mode

brkCurrThr

Current reference during Braking operations

brkSpeedThr

Speed threshold for BRAKE pin and motor stop options (low-side braking or high-side braking or align braking) (% of MAX_SPEED)

actSpinThr

Speed threshold below which motor switches to coasting while stopping motor

2.7 fieldCtrl

Configuration Parameters for Field Control

fieldCtrl

Bit Wise Definition

fluxWeakeningEn

Enable Flux Weakening Algorithm

fluxWeakCurrRatio

Flux Weakening Current Ratio of Id to Iq

fluxWeakeningReference

Reference Modulation Index for Flux Weakening

mtpaEnable

Enable Maximum Torque Per Amp Algorithm

2.8 faultCfg1

Configuration Parameters for faults

faultCfg1

Bit Wise Definition

mtrLckMode

Motor Lock Configuration

lockRetry

retry time span after the Motor Lock Fault is detected

2.9 faultCfg2

Configuration Parameters for faults

faultCfg1

Bit Wise Definition

maxVmMode

Overvoltage fault mode

maxVmMtr

Maximum voltage for running motor

minVmMode

Undervoltage fault mode

minVmMtr

Minimum voltage for running motor

noMtrThr

No motor lock threshold

abnBemfThr

Abnormal BEMF lock threshold (% of expected BEMF)

lockAbnSpeed

Abnormal speed lock threshold (% of MAX_SPEED)

noMtrFaultEn

No motor fault enable

lowBemfFaultEn

Abnormal BEMF enable

abnSpdFaultEn

Abnormal speed enable

2.10 miscAlgo

Configuration Parameters for Miscellaneous Algorithm Configurations Commands

miscAlgo

Bit Wise Definition

brkCurrPersist

Persistence time for declaring motor is stopped after applying brake

isdRunTime

Persistence time for declaring motor is running during Initial Speed Detection

isdStopTime

Persistence time for declaring motor has stopped during Initial Speed Detection

clSlowAcc

Close loop acceleration when estimator is not yet fully aligned

2.11 pinCfg

Configuration Parameters for Miscellaneous Pin Configuration Commands

pinCfg

Bit Wise Definition

brakeInp

Configuration to select Brake Input as PinBased/RegisterBased Align / No Brake

brakePinMode

Enable Low Side Braking / Align Based Braking

vdcFiltDis

DC Bus Voltage filter enable

2.12 periphCfg1

Configuration Parameters for Peripheral Configuration Commands

periphCfg1

Bit Wise Definition

dirChangeMode

Selection of Motor Stop based Reverse startup / Active Spin down based reverse startup

dirInput

DIR pin mode selection from Pin based/Register based Forward Spin/Register based Reverse Spin*

busCurrLimitEnable

Enable the DC bus Current limited to specified Value

busCurrLimit

Maximim Bus Current Limit beyond which modulation index is clamped

mcuDeadTime

Dead Time value in nS

3 UserStatusRegs

Registers for monitoring the algorithm status and algorithm variables

3.1 systemFaultStatus

Shows if any system level fault occurred

3.2 motorState

Shows the state of motor

3.3 VdqFilt

Filtered value of Voltage applied in d and q axis.

VdqFilt

Bit Wise Definition

d

D axis voltage filtered

q

Q axis voltage filtered

Note: Values in fixed point 27 representation.

3.4 currentPI

Shows the KP and KI values used by the D-axis and Q-axis Current controllers.

currentPI

Bit Wise Definition

kp

Float value of proportional constant

ki

Float value of integral constant

3.5 piSpeed

Shows the Reference and feedback values for PI speed controller.

piSpeed

Bit Wise Definition

reference

PI speed Reference

feedback

PI speed Feedback

3.6 piId

Shows the Reference and feedback values for PI ID controller.

piId

Bit Wise Definition

reference

PI id Reference

feedback

PI id Feedback

3.7 piIq

Shows the Reference and feedback values for PI IQ controller.

piIq

Bit Wise Definition

reference

PI iq Reference

feedback

PI iq Feedback

3.8 ipdIdentifiedSector

Sector identified by IPD

3.9 estimatedSpeed

Estimated value of motor speedin perunit. IQ27 value with Max motor speed as base value.

3.10 dcBusVoltage

DC bus voltage value in perunit. IQ27 value with DC Voltage base value as base value.

3.10 torqueLimit

Torque limit value in perunit, this is the Q axis current limit.

3.11 gateDriverFaultStatus

Gate driver faults status register for external reporting

3.12 controllerFaultStatus

Controller fault status register for external reporting

3.13 appVersion

Version of application code

3. API Guide

The Universal FOC API guide provides a detailed description of files, variables, and APIs for the MSPM0 FOC motor control library

4. Supported Devices

DRV8323RS

Supported MSPM0 LaunchPads

Links

DRV8316

Supported MSPM0 LaunchPads

Links

DRV8329

Supported MSPM0 LaunchPads

Links

TIDA010250

Supported reference design

Links

5. Tuning Documentation

For tuning the motor please refer to Tuning Document