MSPM0G3519SensorlessFOCMotorControlLibrary  1.0
Data Fields
ramAlgoDebugCtrl1 Struct Reference

ramAlgoDebugCtrl1 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t reserved1: 10
 
uint32_t forceAlignAngleSrcSelect: 1
 
uint32_t forceISDEn: 1
 
uint32_t forceIPDEn: 1
 
uint32_t forceSlowCycleFirstCycleEn: 1
 
uint32_t forceAlignEn: 1
 
uint32_t closeLoopDis: 1
 
uint32_t reserved: 6
 
uint32_t forcedAlignAngle: 9
 
uint32_t clearFlt: 1
 

Detailed Description

ramAlgoDebugCtrl1 structure

Field Documentation

§ reserved1

uint32_t ramAlgoDebugCtrl1::reserved1

Reserved

§ forceAlignAngleSrcSelect

uint32_t ramAlgoDebugCtrl1::forceAlignAngleSrcSelect

Force align angle state source select

§ forceISDEn

uint32_t ramAlgoDebugCtrl1::forceISDEn

Force ISD enable

§ forceIPDEn

uint32_t ramAlgoDebugCtrl1::forceIPDEn

Force IPD enable

§ forceSlowCycleFirstCycleEn

uint32_t ramAlgoDebugCtrl1::forceSlowCycleFirstCycleEn

Force slow first cycle enable

§ forceAlignEn

uint32_t ramAlgoDebugCtrl1::forceAlignEn

Force align state enable

§ closeLoopDis

uint32_t ramAlgoDebugCtrl1::closeLoopDis

Disable closed loop

§ reserved

uint32_t ramAlgoDebugCtrl1::reserved

Reserved

§ forcedAlignAngle

uint32_t ramAlgoDebugCtrl1::forcedAlignAngle

Align angle used during forced align state

§ clearFlt

uint32_t ramAlgoDebugCtrl1::clearFlt

Clears all faults


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale