MSPM0G3519SensoredFOCMotorControlLibrary  1.0
Data Fields
OVER_CURRENT_T Struct Reference

Over Current Structure. More...

#include <overCurrent.h>

Collaboration diagram for OVER_CURRENT_T:
Collaboration graph
[legend]

Data Fields

int32_t overCurrentLimitSet
 
int32_t overCurrentLimit
 
OVER_CURRENT_FLAGS_T flags
 

Detailed Description

Over Current Structure.

Field Documentation

§ overCurrentLimitSet

int32_t OVER_CURRENT_T::overCurrentLimitSet

OC Limit Set

§ overCurrentLimit

int32_t OVER_CURRENT_T::overCurrentLimit

OC Limit

§ flags

OVER_CURRENT_FLAGS_T OVER_CURRENT_T::flags

The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale