![]() |
![]() |
|
MSPM0C1106HallSensoredTrapMotorControlLibrary
1.0
|
Defines drv8323 instance. More...
#include <drv8323.h>
Defines drv8323 instance.
| HAL_GPIO_OUT DRV8323_Instance::nsleep |
HAL output pin connected to the motor driver's nsleep pin.
Referenced by DRV8323_setnSleep().
| HAL_GPIO_OUT DRV8323_Instance::led |
HAL output pin connected to the motor driver's LED pin
| HAL_GPIO_IN DRV8323_Instance::nfault |
HAL input pin connected to the motor driver's nfault pin.
| _iq20 DRV8323_Instance::csa_sf |
Scale factor used to cache values needed to calculate current
Referenced by DRV8323_getCurrent(), and DRV8323_updateCSAScaleFactor().
| _iq20 DRV8323_Instance::csaVRef |
Scale factor used to cache values needed to calculate current
| HAL_ADC_CHAN DRV8323_Instance::Vsen |
ADc channels used to measure bus voltage
Referenced by DRV8323_init().
| HAL_ADC_CHAN DRV8323_Instance::VsenA |
ADc channels used to measure phase A voltage
Referenced by DRV8323_init().
| HAL_ADC_CHAN DRV8323_Instance::VsenB |
ADc channels used to measure phase B voltage
Referenced by DRV8323_init().
| HAL_ADC_CHAN DRV8323_Instance::VsenC |
ADc channels used to measure phase C voltage
Referenced by DRV8323_init().
| HAL_ADC_CHAN DRV8323_Instance::IsenA |
ADc channels used to measure bus current
Referenced by DRV8323_init().
| HAL_ADC_CHAN DRV8323_Instance::IsenB |
ADc channels used to measure bus current
Referenced by DRV8323_init().
| HAL_ADC_CHAN DRV8323_Instance::IsenC |
ADc channels used to measure bus current
Referenced by DRV8323_init().
| HAL_FAULT_INPUT DRV8323_Instance::faultIn |
pwm timer to which fault pin is connected