EEPROM Library Overview  1.0.0.x
Macros
EEPROM_TYPE_A_STATUS
Collaboration diagram for EEPROM_TYPE_A_STATUS:

Macros

#define EEPROM_EMULATION_WRITE_OK   ((uint32_t) 0x00000000U)
 Data write is successful.
 
#define EEPROM_EMULATION_WRITE_ERROR   ((uint32_t) 0x00000001U)
 Data write failed.
 
#define EEPROM_EMULATION_FORMAT_ERROR   ((uint32_t) 0x00000010U)
 Formatting error.
 
#define EEPROM_EMULATION_INIT_OK   ((uint32_t) 0x00000000U)
 Initialization is successful.
 
#define EEPROM_EMULATION_INIT_ERROR   ((uint32_t) 0x00000002U)
 Initialization failed.
 

Detailed Description

These defines are used for the return status of some commands.

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale