![]() |
![]() |
|
MSPM0L111X TI-Driver Library
2.05.01.00
|
SPI Parameters. More...
#include <SPI.h>

Data Fields | |
| SPI_TransferMode | transferMode |
| uint32_t | transferTimeout |
| SPI_CallbackFxn | transferCallbackFxn |
| SPI_Mode | mode |
| uint32_t | bitRate |
| SPI bit rate in Hz. | |
| uint32_t | dataSize |
| SPI_FrameFormat | frameFormat |
| SPI_Parity | parity |
| SPI_BitOrder | bitOrder |
| void * | custom |
SPI Parameters.
SPI Parameters are used to with the SPI_open() call. Default values for these parameters are set using SPI_Params_init().
| SPI_TransferMode SPI_Params::transferMode |
Blocking or Callback mode
| uint32_t SPI_Params::transferTimeout |
Transfer timeout in system ticks
| SPI_CallbackFxn SPI_Params::transferCallbackFxn |
Callback function pointer
| SPI_Mode SPI_Params::mode |
Controller or Peripheral mode
| uint32_t SPI_Params::dataSize |
SPI data frame size in bits
| SPI_FrameFormat SPI_Params::frameFormat |
SPI frame format
| SPI_Parity SPI_Params::parity |
Parity can be set as even, odd or none
| SPI_BitOrder SPI_Params::bitOrder |
false: MSB first, true: LSB first
| void* SPI_Params::custom |
Custom argument used by driver implementation