MSPM0GX51X TI-Driver Library  2.05.01.00
Data Structures | Functions
Collaboration diagram for I2C driver APIs:

Data Structures

struct  I2CTargetMSPM0_HWAttrs
 I2CTargetMSPM0 Hardware attributes. More...
 
struct  I2CTargetMSPM0_Object
 I2CTargetMSPM0 Object. More...
 

Functions

static bool I2CBaseValid (I2C_Regs *i2c)
 Checks an I2C base address. This function determines if a I2C port base address is valid. More...
 

Detailed Description

Note
All calls should go through the generic I2CTarget API.

Driver Include

The I2CTarget header file should be included in an application as follows:

#include <ti/drivers/i2c/I2CTargetMSPM0.h>

Refer to I2CTarget.h for a complete description of APIs.

Overview

The generic I2CTarget API is normally used in application code, for example, I2CTarget_open(). Do not use APIs in this header file directly. The board file will define the device specific config, and casting in the general API will ensure that the correct device specific functions are called.

General Behavior

Before using the I2C in MSPM0:

Power Management

The Power drivers are yet to implement but the behavior should follow like the information given here. The I2CTargetMSPM0 driver sets a power constraint when I2CTarget_start() is called to keep the device out of standby; so when all tasks are blocked, the device will enter idle mode instead of standby. When the application calls I2CTarget_stop(), the the power constraint to prohibit standby is released. The following statements are valid:

Supported Functions

Note
All calls should go through the generic API.

Use Cases

See generic API for examples.

Function Documentation

§ I2CBaseValid()

static bool I2CBaseValid ( I2C_Regs *  i2c)
static

Checks an I2C base address. This function determines if a I2C port base address is valid.

Parameters
i2cis the base address of the I2C port.
Returns
Returns true if the base address is valid and false otherwise
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale