Overview
Refer to ti_drivers_I2C_Overview for a complete description of APIs and examples of use.
§ I2CSupport_controllerFinish()
| void I2CSupport_controllerFinish |
( |
I2C_HWAttrs const * |
hwAttrs | ) |
|
Function to send a finish command to the controller module.
- Parameters
-
| [in] | hwAttrs | A pointer to an I2C_HWAttrs structure. |
§ I2CSupport_primeTransfer()
Function to initialize transfers.
- Parameters
-
- Returns
- Returns a status indicating success or failure of the transfer.
- Return values
-
| I2C_STATUS_SUCCESS | The transfer was successful. |
| I2C_STATUS_INCOMPLETE | I2C transaction is in progress or returned without completing. |
| I2C_STATUS_BUS_BUSY | I2C bus already in use by another I2C Controller. |