MSPM0GX51X TI-Driver Library  2.05.01.00
Data Structures | Functions
I2CTargetMSPM0.h File Reference

Detailed Description

I2CTarget driver implementation for a MSPM0 device I2C target.


#include <stdint.h>
#include <stdbool.h>
#include <ti/driverlib/dl_i2c.h>
#include <ti/drivers/I2CTarget.h>
Include dependency graph for I2CTargetMSPM0.h:

Go to the source code of this file.

Data Structures

struct  I2CTargetMSPM0_HWAttrs
 I2CTargetMSPM0 Hardware attributes. More...
 
struct  I2CTargetMSPM0_Object
 I2CTargetMSPM0 Object. More...
 

Functions

static bool I2CBaseValid (I2C_Regs *i2c)
 Checks an I2C base address. This function determines if a I2C port base address is valid. More...
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale