MSPM0GX51X Driver Library  2.05.01.00
Modules | Data Structures | Macros | Enumerations | Functions
Direct Memory Access (DMA)
Collaboration diagram for Direct Memory Access (DMA):

Modules

 DL_DMA_INTERRUPT
 
 DL_DMA_EVENT
 

Data Structures

struct  DL_DMA_Config
 Configuration struct for DL_DMA_initChannel. More...
 

Macros

#define DEVICE_HAS_DMA_FULL_CHANNEL
 Device has support for DMA FULL channels.
 
#define DEVICE_HAS_LLONG_ACCESS
 Device has support for DMA 128-bit access on all channels.
 
#define DEVICE_HAS_AUTO_AND_GATHER
 If device has LLONG support, it will also support AUTO reg and GATHER mode.
 

Enumerations

enum  DL_DMA_TRANSFER_MODE {
  DL_DMA_SINGLE_TRANSFER_MODE = DMA_DMACTL_DMATM_SINGLE,
  DL_DMA_SINGLE_BLOCK_TRANSFER_MODE = DMA_DMACTL_DMATM_BLOCK,
  DL_DMA_FULL_CH_REPEAT_SINGLE_TRANSFER_MODE = DMA_DMACTL_DMATM_RPTSNGL,
  DL_DMA_FULL_CH_REPEAT_BLOCK_TRANSFER_MODE = DMA_DMACTL_DMATM_RPTBLCK
}
 
enum  DL_DMA_EXTENDED_MODE {
  DL_DMA_NORMAL_MODE = DMA_DMACTL_DMAEM_NORMAL,
  DL_DMA_FULL_CH_GATHER_MODE = DMA_DMACTL_DMAEM_GATHERMODE,
  DL_DMA_FULL_CH_FILL_MODE = DMA_DMACTL_DMAEM_FILLMODE,
  DL_DMA_FULL_CH_TABLE_MODE = DMA_DMACTL_DMAEM_TABLEMODE
}
 
enum  DL_DMA_INCREMENT {
  DL_DMA_ADDR_UNCHANGED = DMA_DMACTL_DMASRCINCR_UNCHANGED,
  DL_DMA_ADDR_DECREMENT = DMA_DMACTL_DMASRCINCR_DECREMENT,
  DL_DMA_ADDR_INCREMENT = DMA_DMACTL_DMASRCINCR_INCREMENT,
  DL_DMA_ADDR_STRIDE_2 = DMA_DMACTL_DMASRCINCR_STRIDE_2,
  DL_DMA_ADDR_STRIDE_3 = DMA_DMACTL_DMASRCINCR_STRIDE_3,
  DL_DMA_ADDR_STRIDE_4 = DMA_DMACTL_DMASRCINCR_STRIDE_4,
  DL_DMA_ADDR_STRIDE_5 = DMA_DMACTL_DMASRCINCR_STRIDE_5,
  DL_DMA_ADDR_STRIDE_6 = DMA_DMACTL_DMASRCINCR_STRIDE_6,
  DL_DMA_ADDR_STRIDE_7 = DMA_DMACTL_DMASRCINCR_STRIDE_7,
  DL_DMA_ADDR_STRIDE_8 = DMA_DMACTL_DMASRCINCR_STRIDE_8,
  DL_DMA_ADDR_STRIDE_9 = DMA_DMACTL_DMASRCINCR_STRIDE_9
}
 
enum  DL_DMA_EARLY_INTERRUPT_THRESHOLD {
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_DISABLED = DMA_DMACTL_DMAPREIRQ_PREIRQ_DISABLE,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_1 = DMA_DMACTL_DMAPREIRQ_PREIRQ_1,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_2 = DMA_DMACTL_DMAPREIRQ_PREIRQ_2,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_4 = DMA_DMACTL_DMAPREIRQ_PREIRQ_4,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_8 = DMA_DMACTL_DMAPREIRQ_PREIRQ_8,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_32 = DMA_DMACTL_DMAPREIRQ_PREIRQ_32,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_64 = DMA_DMACTL_DMAPREIRQ_PREIRQ_64,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_HALF = DMA_DMACTL_DMAPREIRQ_PREIRQ_HALF
}
 
enum  DL_DMA_BURST_SIZE {
  DL_DMA_BURST_SIZE_INFINITY = DMA_DMAPRIO_BURSTSZ_INFINITI,
  DL_DMA_BURST_SIZE_8 = DMA_DMAPRIO_BURSTSZ_BURST_8,
  DL_DMA_BURST_SIZE_16 = DMA_DMAPRIO_BURSTSZ_BUSRT_16,
  DL_DMA_BURST_SIZE_32 = DMA_DMAPRIO_BURSTSZ_BURST_32
}
 
enum  DL_DMA_TRIGGER_TYPE {
  DL_DMA_TRIGGER_TYPE_INTERNAL = DMA_DMATCTL_DMATINT_INTERNAL,
  DL_DMA_TRIGGER_TYPE_EXTERNAL = DMA_DMATCTL_DMATINT_EXTERNAL
}
 
enum  DL_DMA_WIDTH {
  DL_DMA_WIDTH_BYTE = DMA_DMACTL_DMASRCWDTH_BYTE,
  DL_DMA_WIDTH_HALF_WORD = DMA_DMACTL_DMASRCWDTH_HALF,
  DL_DMA_WIDTH_WORD = DMA_DMACTL_DMASRCWDTH_WORD,
  DL_DMA_WIDTH_LONG = DMA_DMACTL_DMASRCWDTH_LONG,
  DL_DMA_WIDTH_LONG_LONG = DMA_DMACTL_DMASRCWDTH_LONGLONG
}
 
enum  DL_DMA_EVENT_IIDX {
  DL_DMA_EVENT_IIDX_NO_INTR = DMA_GEN_EVENT_IIDX_STAT_NO_INTR,
  DL_DMA_EVENT_IIDX_DMACH0 = DMA_GEN_EVENT_IIDX_STAT_DMACH0,
  DL_DMA_EVENT_IIDX_DMACH1 = DMA_GEN_EVENT_IIDX_STAT_DMACH1,
  DL_DMA_EVENT_IIDX_DMACH2 = DMA_GEN_EVENT_IIDX_STAT_DMACH2,
  DL_DMA_EVENT_IIDX_DMACH3 = DMA_GEN_EVENT_IIDX_STAT_DMACH3,
  DL_DMA_EVENT_IIDX_DMACH4 = DMA_GEN_EVENT_IIDX_STAT_DMACH4,
  DL_DMA_EVENT_IIDX_DMACH5 = DMA_GEN_EVENT_IIDX_STAT_DMACH5,
  DL_DMA_EVENT_IIDX_DMACH6 = DMA_GEN_EVENT_IIDX_STAT_DMACH6,
  DL_DMA_EVENT_IIDX_DMACH7 = DMA_GEN_EVENT_IIDX_STAT_DMACH7,
  DL_DMA_EVENT_IIDX_DMACH8 = DMA_GEN_EVENT_IIDX_STAT_DMACH8,
  DL_DMA_EVENT_IIDX_DMACH9 = DMA_GEN_EVENT_IIDX_STAT_DMACH9,
  DL_DMA_EVENT_IIDX_DMACH10 = DMA_GEN_EVENT_IIDX_STAT_DMACH10,
  DL_DMA_EVENT_IIDX_DMACH11 = DMA_GEN_EVENT_IIDX_STAT_DMACH11,
  DL_DMA_EVENT_IIDX_DMACH12 = DMA_GEN_EVENT_IIDX_STAT_DMACH12,
  DL_DMA_EVENT_IIDX_DMACH13 = DMA_GEN_EVENT_IIDX_STAT_DMACH13,
  DL_DMA_EVENT_IIDX_DMACH14 = DMA_GEN_EVENT_IIDX_STAT_DMACH14,
  DL_DMA_EVENT_IIDX_DMACH15 = DMA_GEN_EVENT_IIDX_STAT_DMACH15,
  DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH0 = DMA_GEN_EVENT_IIDX_STAT_PREIRQCH0,
  DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH1 = DMA_GEN_EVENT_IIDX_STAT_PREIRQCH1,
  DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH2 = DMA_GEN_EVENT_IIDX_STAT_PREIRQCH2,
  DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH3 = DMA_GEN_EVENT_IIDX_STAT_PREIRQCH3,
  DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH4 = DMA_GEN_EVENT_IIDX_STAT_PREIRQCH4,
  DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH5 = DMA_GEN_EVENT_IIDX_STAT_PREIRQCH5,
  DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH6 = DMA_GEN_EVENT_IIDX_STAT_PREIRQCH6,
  DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH7 = DMA_GEN_EVENT_IIDX_STAT_PREIRQCH7,
  DL_DMA_EVENT_IIDX_ADDR_ERROR = DMA_GEN_EVENT_IIDX_STAT_ADDRERR,
  DL_DMA_EVENT_IIDX_DATA_ERROR = DMA_GEN_EVENT_IIDX_STAT_DATAERR
}
 
enum  DL_DMA_PUBLISHER_INDEX { DL_DMA_PUBLISHER_INDEX_0 = 0 }
 
enum  DL_DMA_SUBSCRIBER_INDEX {
  DL_DMA_SUBSCRIBER_INDEX_0 = 0,
  DL_DMA_SUBSCRIBER_INDEX_1 = 1
}
 
enum  DL_DMA_AUTOEN {
  DL_DMA_AUTOEN_DISABLE = DMA_DMACTL_DMAAUTOEN_DISABLE,
  DL_DMA_AUTOEN_DMASA = DMA_DMACTL_DMAAUTOEN_DMASA,
  DL_DMA_AUTOEN_DMADA = DMA_DMACTL_DMAAUTOEN_DMADA,
  DL_DMA_AUTOEN_DMASZ = DMA_DMACTL_DMAAUTOEN_DMASZ
}
 

Functions

void DL_DMA_initChannel (DMA_Regs *dma, uint8_t channelNum, const DL_DMA_Config *config)
 Initialize a DMA channel. More...
 
__STATIC_INLINE void DL_DMA_configTransfer (DMA_Regs *dma, uint8_t channelNum, DL_DMA_TRANSFER_MODE transferMode, DL_DMA_EXTENDED_MODE extendedMode, DL_DMA_WIDTH srcWidth, DL_DMA_WIDTH destWidth, DL_DMA_INCREMENT srcIncrement, DL_DMA_INCREMENT destIncrement)
 Configure a DMA channel for a transfer. More...
 
__STATIC_INLINE void DL_DMA_enableRoundRobinPriority (DMA_Regs *dma)
 Configure the DMA for round-robin priority. More...
 
__STATIC_INLINE void DL_DMA_disableRoundRobinPriority (DMA_Regs *dma)
 Disable round-robin priority for the DMA. More...
 
__STATIC_INLINE bool DL_DMA_isRoundRobinPriorityEnabled (const DMA_Regs *dma)
 Check if round-robin priority is enabled for the DMA. More...
 
__STATIC_INLINE void DL_DMA_setBurstSize (DMA_Regs *dma, DL_DMA_BURST_SIZE burstSize)
 Set the burst size for block transfers. More...
 
__STATIC_INLINE DL_DMA_BURST_SIZE DL_DMA_getBurstSize (const DMA_Regs *dma)
 Get the burst size for block transfers. More...
 
__STATIC_INLINE void DL_DMA_enableChannel (DMA_Regs *dma, uint8_t channelNum)
 Enable a DMA channel for transfers. More...
 
__STATIC_INLINE void DL_DMA_disableChannel (DMA_Regs *dma, uint8_t channelNum)
 Disable a DMA channel for transfers. More...
 
__STATIC_INLINE bool DL_DMA_isChannelEnabled (const DMA_Regs *dma, uint8_t channelNum)
 Check if a DMA channel is enabled for transfers. More...
 
__STATIC_INLINE void DL_DMA_configMode (DMA_Regs *dma, uint8_t channelNum, DL_DMA_TRANSFER_MODE transferMode, DL_DMA_EXTENDED_MODE extendedMode)
 Configure the mode for a DMA channel. More...
 
__STATIC_INLINE void DL_DMA_setTransferMode (DMA_Regs *dma, uint8_t channelNum, DL_DMA_TRANSFER_MODE transferMode)
 Set a DMA channel's transfer mode. More...
 
__STATIC_INLINE DL_DMA_TRANSFER_MODE DL_DMA_getTransferMode (const DMA_Regs *dma, uint8_t channelNum)
 Get a DMA channel's transfer mode. More...
 
__STATIC_INLINE void DL_DMA_setExtendedMode (DMA_Regs *dma, uint8_t channelNum, DL_DMA_EXTENDED_MODE extendedMode)
 Set a DMA channel's extended mode. More...
 
__STATIC_INLINE DL_DMA_EXTENDED_MODE DL_DMA_getExtendedMode (const DMA_Regs *dma, uint8_t channelNum)
 Get a DMA channel's extended mode. More...
 
__STATIC_INLINE void DL_DMA_startTransfer (DMA_Regs *dma, uint8_t channelNum)
 Start a DMA transfer using software. More...
 
__STATIC_INLINE void DL_DMA_setTrigger (DMA_Regs *dma, uint8_t channelNum, uint8_t trigger, DL_DMA_TRIGGER_TYPE triggerType)
 Set a channel's trigger for a DMA transfer. More...
 
__STATIC_INLINE uint32_t DL_DMA_getTrigger (const DMA_Regs *dma, uint8_t channelNum)
 Get the current trigger for a DMA channel. More...
 
__STATIC_INLINE DL_DMA_TRIGGER_TYPE DL_DMA_getTriggerType (const DMA_Regs *dma, uint8_t channelNum)
 Get the current trigger type for a DMA channel. More...
 
__STATIC_INLINE void DL_DMA_setSrcAddr (DMA_Regs *dma, uint8_t channelNum, uint32_t srcAddr)
 Set a DMA channel's source address. More...
 
__STATIC_INLINE uint32_t DL_DMA_getSrcAddr (const DMA_Regs *dma, uint8_t channelNum)
 Get a DMA channel's source address. More...
 
__STATIC_INLINE void DL_DMA_setDestAddr (DMA_Regs *dma, uint8_t channelNum, uint32_t destAddr)
 Set a DMA channel's destination address. More...
 
__STATIC_INLINE uint32_t DL_DMA_getDestAddr (const DMA_Regs *dma, uint8_t channelNum)
 Get a DMA channel's destination address. More...
 
__STATIC_INLINE void DL_DMA_setTransferSize (DMA_Regs *dma, uint8_t channelNum, uint16_t size)
 Set the size of a block for a DMA transfer. More...
 
__STATIC_INLINE uint16_t DL_DMA_getTransferSize (const DMA_Regs *dma, uint8_t channelNum)
 Get a channel's size of block of data for a DMA transfer. More...
 
__STATIC_INLINE void DL_DMA_setSrcIncrement (DMA_Regs *dma, uint8_t channelNum, DL_DMA_INCREMENT srcIncrement)
 Set a channel's source address increment amount. More...
 
__STATIC_INLINE DL_DMA_INCREMENT DL_DMA_getSrcIncrement (const DMA_Regs *dma, uint8_t channelNum)
 Return a channel's source address increment amount. More...
 
__STATIC_INLINE void DL_DMA_setDestIncrement (DMA_Regs *dma, uint8_t channelNum, DL_DMA_INCREMENT destIncrement)
 Set a channel's destination address increment amount. More...
 
__STATIC_INLINE DL_DMA_INCREMENT DL_DMA_getDestIncrement (const DMA_Regs *dma, uint8_t channelNum)
 Return a channel's destination address increment amount. More...
 
__STATIC_INLINE void DL_DMA_setSrcWidth (DMA_Regs *dma, uint8_t channelNum, DL_DMA_WIDTH srcWidth)
 Set the width of the DMA source address for a channel. More...
 
__STATIC_INLINE DL_DMA_WIDTH DL_DMA_getSrcWidth (const DMA_Regs *dma, uint8_t channelNum)
 Get the width of the DMA source address for a channel. More...
 
__STATIC_INLINE void DL_DMA_setDestWidth (DMA_Regs *dma, uint8_t channelNum, DL_DMA_WIDTH destWidth)
 Set the width of the DMA destination address for a channel. More...
 
__STATIC_INLINE DL_DMA_WIDTH DL_DMA_getDestWidth (const DMA_Regs *dma, uint8_t channelNum)
 Get the width of the DMA destination address for a channel. More...
 
__STATIC_INLINE void DL_DMA_Full_Ch_setEarlyInterruptThreshold (DMA_Regs *dma, uint8_t channelNum, DL_DMA_EARLY_INTERRUPT_THRESHOLD threshold)
 Set the early interrupt event. More...
 
__STATIC_INLINE DL_DMA_EARLY_INTERRUPT_THRESHOLD DL_DMA_Full_Ch_getEarlyInterruptThreshold (const DMA_Regs *dma, uint8_t channelNum)
 Get the early interrupt event threshold. More...
 
__STATIC_INLINE void DL_DMA_enableInterrupt (DMA_Regs *dma, uint32_t interruptMask)
 Enable DMA interrupts. More...
 
__STATIC_INLINE void DL_DMA_disableInterrupt (DMA_Regs *dma, uint32_t interruptMask)
 Disable DMA interrupts. More...
 
__STATIC_INLINE uint32_t DL_DMA_getEnabledInterrupts (const DMA_Regs *dma, uint32_t interruptMask)
 Check which DMA interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_DMA_getEnabledInterruptStatus (const DMA_Regs *dma, uint32_t interruptMask)
 Check interrupt flag of enabled DMA interrupts. More...
 
__STATIC_INLINE uint32_t DL_DMA_getRawInterruptStatus (const DMA_Regs *dma, uint32_t interruptMask)
 Check interrupt flag of any DMA interrupt. More...
 
__STATIC_INLINE DL_DMA_EVENT_IIDX DL_DMA_getPendingInterrupt (const DMA_Regs *dma)
 Get highest priority pending DMA interrupt. More...
 
__STATIC_INLINE void DL_DMA_clearInterruptStatus (DMA_Regs *dma, uint32_t interruptMask)
 Clear pending DMA interrupts. More...
 
__STATIC_INLINE void DL_DMA_setPublisherChanID (DMA_Regs *dma, DL_DMA_PUBLISHER_INDEX index, uint8_t chanID)
 Sets the event publisher channel id. More...
 
__STATIC_INLINE uint8_t DL_DMA_getPublisherChanID (DMA_Regs *dma, DL_DMA_PUBLISHER_INDEX index)
 Gets the event publisher channel id. More...
 
__STATIC_INLINE void DL_DMA_setSubscriberChanID (DMA_Regs *dma, DL_DMA_SUBSCRIBER_INDEX index, uint8_t chanID)
 Sets the event subscriber channel id. More...
 
__STATIC_INLINE uint8_t DL_DMA_getSubscriberChanID (DMA_Regs *dma, DL_DMA_SUBSCRIBER_INDEX index)
 Gets the event subscriber channel id. More...
 
__STATIC_INLINE void DL_DMA_enableEvent (DMA_Regs *dma, uint32_t eventMask)
 Enable DMA event. More...
 
__STATIC_INLINE void DL_DMA_disableEvent (DMA_Regs *dma, uint32_t eventMask)
 Disable DMA event. More...
 
__STATIC_INLINE uint32_t DL_DMA_getEnabledEvents (const DMA_Regs *dma, uint32_t eventMask)
 Check which dma events triggers are enabled. More...
 
__STATIC_INLINE uint32_t DL_DMA_getEnabledEventStatus (const DMA_Regs *dma, uint32_t eventMask)
 Check event flag of enabled dma event. More...
 
__STATIC_INLINE uint32_t DL_DMA_getRawEventsStatus (const DMA_Regs *dma, uint32_t eventMask)
 Check event flag of any dma event. More...
 
__STATIC_INLINE void DL_DMA_clearEventsStatus (DMA_Regs *dma, uint32_t eventMask)
 Clear pending dma events. More...
 
__STATIC_INLINE void DL_DMA_enableAutoEnable (DMA_Regs *dma, DL_DMA_AUTOEN mode, uint8_t channelNum)
 Configure the DMA for auto-enable. More...
 
__STATIC_INLINE void DL_DMA_disableAutoEnable (DMA_Regs *dma, uint8_t channelNum)
 Disable auto-enable for DMA. More...
 
__STATIC_INLINE bool DL_DMA_isAutoEnableEnabled (const DMA_Regs *dma, uint8_t channelNum)
 Check if auto-enable is enabled for the DMA. More...
 

Detailed Description

Overview

The Direct Memory Access (DMA) Library allows full configuration of the MSPM0 DMA module. The DMA controller transfers data from one address to another, without CPU intervention, across the entire address range. DMA controllers have multiple channels that can be configured independently

Enumeration Type Documentation

§ DL_DMA_TRANSFER_MODE

Enumerator
DL_DMA_SINGLE_TRANSFER_MODE 

Each DMA trigger results in a single data transfer, once

DL_DMA_SINGLE_BLOCK_TRANSFER_MODE 

Each DMA trigger results in a transfer of a block of data, once

DL_DMA_FULL_CH_REPEAT_SINGLE_TRANSFER_MODE 

Available for FULL-channel configuration only. Each DMA trigger results in a single data transfer, repeating

DL_DMA_FULL_CH_REPEAT_BLOCK_TRANSFER_MODE 

Available for FULL-channel configuration only. Each DMA trigger results in a transfer of a block of data, repeating

§ DL_DMA_EXTENDED_MODE

Enumerator
DL_DMA_NORMAL_MODE 

Normal operation

DL_DMA_FULL_CH_GATHER_MODE 

Available for FULL-channel configuration only. Reads data from address table located at source address and transfers data to destination address

DL_DMA_FULL_CH_FILL_MODE 

Available for FULL-channel configuration only. Fills the destination with a specific value

DL_DMA_FULL_CH_TABLE_MODE 

Available for FULL-channel configuration only. The source data contains addresses and data

§ DL_DMA_INCREMENT

Enumerator
DL_DMA_ADDR_UNCHANGED 

Do not change address after each transfer

DL_DMA_ADDR_DECREMENT 

Decrement address by 1 * DL_DMA_WIDTH after each transfer

DL_DMA_ADDR_INCREMENT 

Increment address by 1 * DL_DMA_WIDTH after each transfer

DL_DMA_ADDR_STRIDE_2 

Stride mode 2, increment address by 2 * DL_DMA_WIDTH (skip over every other element)

DL_DMA_ADDR_STRIDE_3 

Stride mode 3, increment address by 3 * DL_DMA_WIDTH (skip over two elements

DL_DMA_ADDR_STRIDE_4 

Stride mode 4, increment address by 4 * DL_DMA_WIDTH (skip over three elements

DL_DMA_ADDR_STRIDE_5 

Stride mode 5, increment address by 5 * DL_DMA_WIDTH (skip over four elements

DL_DMA_ADDR_STRIDE_6 

Stride mode 6, increment address by 6 * DL_DMA_WIDTH (skip over five elements

DL_DMA_ADDR_STRIDE_7 

Stride mode 7, increment address by 7 * DL_DMA_WIDTH (skip over six elements

DL_DMA_ADDR_STRIDE_8 

Stride mode 8, increment address by 8 * DL_DMA_WIDTH (skip over seven elements

DL_DMA_ADDR_STRIDE_9 

Stride mode 9, increment address by 9 * DL_DMA_WIDTH (skip over eight elements

§ DL_DMA_EARLY_INTERRUPT_THRESHOLD

Enumerator
DL_DMA_EARLY_INTERRUPT_THRESHOLD_DISABLED 

Disable early interrupt events

DL_DMA_EARLY_INTERRUPT_THRESHOLD_1 

Generate Early-IRQ event with one transfer pending (DMASZ=1)

DL_DMA_EARLY_INTERRUPT_THRESHOLD_2 

Generate Early-IRQ event with two transfers pending (DMASZ=2)

DL_DMA_EARLY_INTERRUPT_THRESHOLD_4 

Generate Early-IRQ event with three transfers pending (DMASZ=4)

DL_DMA_EARLY_INTERRUPT_THRESHOLD_8 

Generate Early-IRQ event with eight transfers pending (DMASZ=8)

DL_DMA_EARLY_INTERRUPT_THRESHOLD_32 

Generate Early-IRQ event with 32 transfers pending (DMASZ=32)

DL_DMA_EARLY_INTERRUPT_THRESHOLD_64 

Generate Early-IRQ event with 64 transfers pending (DMASZ=64)

DL_DMA_EARLY_INTERRUPT_THRESHOLD_HALF 

Generate Early-IRQ event when DMASZ reaches the half size point of the original transfer size

§ DL_DMA_BURST_SIZE

Enumerator
DL_DMA_BURST_SIZE_INFINITY 

No burst interruption. The block transfer always transfers all elements defined in the DMASZ register before priority is newly evaluated

DL_DMA_BURST_SIZE_8 

Burst size of a block transfer is 8

DL_DMA_BURST_SIZE_16 

Burst size of a block transfer is 16

DL_DMA_BURST_SIZE_32 

Burst size of a block transfer is 32

§ DL_DMA_TRIGGER_TYPE

Enumerator
DL_DMA_TRIGGER_TYPE_INTERNAL 

Internal DMA channel is selected as the DMA trigger

DL_DMA_TRIGGER_TYPE_EXTERNAL 

External DMA channel is selected as the DMA trigger

§ DL_DMA_WIDTH

Enumerator
DL_DMA_WIDTH_BYTE 

Byte Acccess (8-bit)

DL_DMA_WIDTH_HALF_WORD 

Half Word Acccess (16-bit)

DL_DMA_WIDTH_WORD 

Word Acccess (32-bit)

DL_DMA_WIDTH_LONG 

Long Acccess (64-bit)

DL_DMA_WIDTH_LONG_LONG 

Long-long Acccess (128-bit)

§ DL_DMA_EVENT_IIDX

Enumerator
DL_DMA_EVENT_IIDX_NO_INTR 

Enum to indicate that no DMA event has taken place

DL_DMA_EVENT_IIDX_DMACH0 

Enum to indicate that the channel 0 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH1 

Enum to indicate that the channel 1 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH2 

Enum to indicate that the channel 2 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH3 

Enum to indicate that the channel 3 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH4 

Enum to indicate that the channel 4 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH5 

Enum to indicate that the channel 5 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH6 

Enum to indicate that the channel 6 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH7 

Enum to indicate that the channel 7 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH8 

Enum to indicate that the channel 8 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH9 

Enum to indicate that the channel 9 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH10 

Enum to indicate that the channel 10 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH11 

Enum to indicate that the channel 11 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH12 

Enum to indicate that the channel 12 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH13 

Enum to indicate that the channel 13 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH14 

Enum to indicate that the channel 14 interrupt has fired

DL_DMA_EVENT_IIDX_DMACH15 

Enum to indicate that the channel 15 interrupt has fired

DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH0 

Available for FULL-channel configuration only. Enum to indicate that the early interrupt event for channel 0 interrupt has fired

DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH1 

Available for FULL-channel configuration only. Enum to indicate that the early interrupt event for channel 1 interrupt has fired

DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH2 

Available for FULL-channel configuration only. Enum to indicate that the early interrupt event for channel 2 interrupt has fired

DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH3 

Available for FULL-channel configuration only. Enum to indicate that the early interrupt event for channel 3 interrupt has fired

DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH4 

Available for FULL-channel configuration only. Enum to indicate that the early interrupt event for channel 4 interrupt has fired

DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH5 

Available for FULL-channel configuration only. Enum to indicate that the early interrupt event for channel 5 interrupt has fired

DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH6 

Available for FULL-channel configuration only. Enum to indicate that the early interrupt event for channel 6 interrupt has fired

DL_DMA_FULL_CH_EVENT_IIDX_EARLY_IRQ_DMACH7 

Available for FULL-channel configuration only. Enum to indicate that the early interrupt event for channel 7 interrupt has fired

DL_DMA_EVENT_IIDX_ADDR_ERROR 

Enum to indicate that a DMA address error has occurred

DL_DMA_EVENT_IIDX_DATA_ERROR 

Enum to indicate that a DMA data error has occurred

§ DL_DMA_PUBLISHER_INDEX

Enumerator
DL_DMA_PUBLISHER_INDEX_0 

DMA Publisher index 0

§ DL_DMA_SUBSCRIBER_INDEX

Enumerator
DL_DMA_SUBSCRIBER_INDEX_0 

DMA Subscriber index 0

DL_DMA_SUBSCRIBER_INDEX_1 

DMA Subscriber index 1

§ DL_DMA_AUTOEN

Enumerator
DL_DMA_AUTOEN_DISABLE 

No automatic DMA enable

DL_DMA_AUTOEN_DMASA 

Automatic DMA enable on DMASA register write

DL_DMA_AUTOEN_DMADA 

Automatic DMA enable on DMADA register write

DL_DMA_AUTOEN_DMASZ 

Automatic DMA enable on DMASZ register write

Function Documentation

§ DL_DMA_initChannel()

void DL_DMA_initChannel ( DMA_Regs *  dma,
uint8_t  channelNum,
const DL_DMA_Config config 
)

Initialize a DMA channel.

Initializes all the configurable options for a DMA channel. The DMA channel is not enabled in this API.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]configPointer to DMA channel configuration settings

§ DL_DMA_configTransfer()

__STATIC_INLINE void DL_DMA_configTransfer ( DMA_Regs *  dma,
uint8_t  channelNum,
DL_DMA_TRANSFER_MODE  transferMode,
DL_DMA_EXTENDED_MODE  extendedMode,
DL_DMA_WIDTH  srcWidth,
DL_DMA_WIDTH  destWidth,
DL_DMA_INCREMENT  srcIncrement,
DL_DMA_INCREMENT  destIncrement 
)

Configure a DMA channel for a transfer.

Configures the transfer settings for a DMA channel. The DMA channel is not enabled in this API.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]transferModeThe transfer mode to use. Refer to the device datasheet to determine which modes are supported in the selected channel. One of DL_DMA_TRANSFER_MODE.
[in]extendedModeThe extended mode to use. One of DL_DMA_EXTENDED_MODE.
[in]srcWidthThe width of the DMA source. One of DL_DMA_WIDTH.
[in]destWidthThe width of the DMA destination. One of DL_DMA_WIDTH.
[in]srcIncrementAmount to increment/decrement the DMA source address by. One of DL_DMA_INCREMENT.
[in]destIncrementAmount to increment/decrement the DMA destination address by. One of DL_DMA_INCREMENT.

§ DL_DMA_enableRoundRobinPriority()

__STATIC_INLINE void DL_DMA_enableRoundRobinPriority ( DMA_Regs *  dma)

Configure the DMA for round-robin priority.

When round-robin priority is enabled, the channel that completes a transfer becomes the lowest priority. If multiple triggers happen simultaneously or are pending, the channel that transferred least recently will transfer first. Once it's complete the next highest priority channel will transfer.

Parameters
[in]dmaPointer to the register overlay for the peripheral

§ DL_DMA_disableRoundRobinPriority()

__STATIC_INLINE void DL_DMA_disableRoundRobinPriority ( DMA_Regs *  dma)

Disable round-robin priority for the DMA.

When round-robin priority is disabled, the channel priorities are fixed in ascending order (Channel 0 is the lowed priority). If multiple triggers happen simultaneously or are pending, the channel with the highest priority completes its transfer before the next-highest transfer can start.

Parameters
[in]dmaPointer to the register overlay for the peripheral

§ DL_DMA_isRoundRobinPriorityEnabled()

__STATIC_INLINE bool DL_DMA_isRoundRobinPriorityEnabled ( const DMA_Regs *  dma)

Check if round-robin priority is enabled for the DMA.

Parameters
[in]dmaPointer to the register overlay for the peripheral
Returns
The status of round-robin priority
Return values
trueRound-robin priority is enabled
falseRound-robin priority is disabled

§ DL_DMA_setBurstSize()

__STATIC_INLINE void DL_DMA_setBurstSize ( DMA_Regs *  dma,
DL_DMA_BURST_SIZE  burstSize 
)

Set the burst size for block transfers.

After the DMA transfers the amount of transfers defined by DL_DMA_BURST_SIZE, the ongoing block transfer is interrupted and the priority encoder has the chance to assign a higher priority channel. The previously interrupted block transfer is internally marked as pending and when no other high priority channel is pending the block transfer will continue with the next burst or until DMASZ counts down to 0.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]burstSizeThe burst size to set. One of DL_DMA_BURST_SIZE.
See also
DL_DMA_configTransfer

References DL_Common_updateReg().

§ DL_DMA_getBurstSize()

__STATIC_INLINE DL_DMA_BURST_SIZE DL_DMA_getBurstSize ( const DMA_Regs *  dma)

Get the burst size for block transfers.

Parameters
[in]dmaPointer to the register overlay for the peripheral
Returns
The burst size for block transfers
Return values
Oneof DL_DMA_BURST_SIZE

§ DL_DMA_enableChannel()

__STATIC_INLINE void DL_DMA_enableChannel ( DMA_Regs *  dma,
uint8_t  channelNum 
)

Enable a DMA channel for transfers.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on

§ DL_DMA_disableChannel()

__STATIC_INLINE void DL_DMA_disableChannel ( DMA_Regs *  dma,
uint8_t  channelNum 
)

Disable a DMA channel for transfers.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on

§ DL_DMA_isChannelEnabled()

__STATIC_INLINE bool DL_DMA_isChannelEnabled ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Check if a DMA channel is enabled for transfers.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
The status of the DMA channel
Return values
trueThe DMA channel is enabled
falseThe DMA channel is disabled

§ DL_DMA_configMode()

__STATIC_INLINE void DL_DMA_configMode ( DMA_Regs *  dma,
uint8_t  channelNum,
DL_DMA_TRANSFER_MODE  transferMode,
DL_DMA_EXTENDED_MODE  extendedMode 
)

Configure the mode for a DMA channel.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]transferModeThe transfer mode to set for the channel. Refer to the device datasheet to determine which modes are supported in the selected channel. One of DL_DMA_TRANSFER_MODE.
[in]extendedModeThe extended operation mode to set for the channel. One of DL_DMA_EXTENDED_MODE.
See also
DL_DMA_configTransfer

References DL_Common_updateReg().

§ DL_DMA_setTransferMode()

__STATIC_INLINE void DL_DMA_setTransferMode ( DMA_Regs *  dma,
uint8_t  channelNum,
DL_DMA_TRANSFER_MODE  transferMode 
)

Set a DMA channel's transfer mode.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]transferModeThe transfer mode to use. Refer to the device datasheet to determine which modes are supported in the selected channel. One of DL_DMA_TRANSFER_MODE.
See also
DL_DMA_configMode
DL_DMA_configTransfer

References DL_Common_updateReg().

§ DL_DMA_getTransferMode()

__STATIC_INLINE DL_DMA_TRANSFER_MODE DL_DMA_getTransferMode ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Get a DMA channel's transfer mode.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
The channel's transfer mode
Return values
Oneof DL_DMA_TRANSFER_MODE

§ DL_DMA_setExtendedMode()

__STATIC_INLINE void DL_DMA_setExtendedMode ( DMA_Regs *  dma,
uint8_t  channelNum,
DL_DMA_EXTENDED_MODE  extendedMode 
)

Set a DMA channel's extended mode.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]extendedModeThe transfer mode to use. One of DL_DMA_EXTENDED_MODE.
See also
DL_DMA_configMode
DL_DMA_configTransfer

References DL_Common_updateReg().

§ DL_DMA_getExtendedMode()

__STATIC_INLINE DL_DMA_EXTENDED_MODE DL_DMA_getExtendedMode ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Get a DMA channel's extended mode.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
The channel's transfer mode
Return values
Oneof DL_DMA_EXTENDED_MODE

§ DL_DMA_startTransfer()

__STATIC_INLINE void DL_DMA_startTransfer ( DMA_Regs *  dma,
uint8_t  channelNum 
)

Start a DMA transfer using software.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on

§ DL_DMA_setTrigger()

__STATIC_INLINE void DL_DMA_setTrigger ( DMA_Regs *  dma,
uint8_t  channelNum,
uint8_t  trigger,
DL_DMA_TRIGGER_TYPE  triggerType 
)

Set a channel's trigger for a DMA transfer.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]triggerWhat should trigger a DMA transfer. Refer to the datasheet of the device for which DMA trigger values map to which events.
[in]triggerTypeWhether an internal or external DMA channel is selected as the DMA trigger. Refer to the datasheet for more information on the DMA channels.

References DL_Common_updateReg().

§ DL_DMA_getTrigger()

__STATIC_INLINE uint32_t DL_DMA_getTrigger ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Get the current trigger for a DMA channel.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
What is configured to trigger a DMA transfer.
Return values
Checkthe device datasheet for what values are mapped to on your device.

§ DL_DMA_getTriggerType()

__STATIC_INLINE DL_DMA_TRIGGER_TYPE DL_DMA_getTriggerType ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Get the current trigger type for a DMA channel.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
Whether an internal or external DMA channel is selected as the DMA trigger.
Return values
Oneof DL_DMA_TRIGGER_TYPE

§ DL_DMA_setSrcAddr()

__STATIC_INLINE void DL_DMA_setSrcAddr ( DMA_Regs *  dma,
uint8_t  channelNum,
uint32_t  srcAddr 
)

Set a DMA channel's source address.

Set the source address for a DMA channel for transferring data from. This address can be automatically incremented/decremented after the completion of a transfer by using the DL_DMA_setSrcIncrement function.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]srcAddrAddress to set as the DMA source
See also
DL_DMA_setSrcIncrement

§ DL_DMA_getSrcAddr()

__STATIC_INLINE uint32_t DL_DMA_getSrcAddr ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Get a DMA channel's source address.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
Source address for the DMA channel

§ DL_DMA_setDestAddr()

__STATIC_INLINE void DL_DMA_setDestAddr ( DMA_Regs *  dma,
uint8_t  channelNum,
uint32_t  destAddr 
)

Set a DMA channel's destination address.

Set the destination address for a DMA channel for transferring data to. This address can be automatically incremented/decremented after the completion of a transfer by using the DL_DMA_setDestIncrement function.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]destAddrAddress to set as the DMA destination
See also
DL_DMA_setDestIncrement

§ DL_DMA_getDestAddr()

__STATIC_INLINE uint32_t DL_DMA_getDestAddr ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Get a DMA channel's destination address.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
Destination address for the DMA channel

§ DL_DMA_setTransferSize()

__STATIC_INLINE void DL_DMA_setTransferSize ( DMA_Regs *  dma,
uint8_t  channelNum,
uint16_t  size 
)

Set the size of a block for a DMA transfer.

Defines the size of the block of data to transfer.

When the transfer mode DL_DMA_TRANSFER_MODE is a Block transfer mode, this is the size of the block of data transferred every trigger.

When in the transfer mode DL_DMA_TRANSFER_MODE is a Single transfer mode, this is how many triggers need to occur before the block is considered done, which then sets the interrupt status.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]sizeThe size of the block of data to transfer. Value between 0 - 65535.

§ DL_DMA_getTransferSize()

__STATIC_INLINE uint16_t DL_DMA_getTransferSize ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Get a channel's size of block of data for a DMA transfer.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
The channel's size of block of data to transfer
Return values
Avalue between 0 - 65535.

§ DL_DMA_setSrcIncrement()

__STATIC_INLINE void DL_DMA_setSrcIncrement ( DMA_Regs *  dma,
uint8_t  channelNum,
DL_DMA_INCREMENT  srcIncrement 
)

Set a channel's source address increment amount.

After each DMA transfer the channel source address, which can be set by DL_DMA_setSrcAddr, can be incremented, decremented or remain unchanged. This controls if the DMA is copying from a fixed address or a block of addresses.

The amount that is incremented/decremented is controlled by the width of the source, set by DL_DMA_setSrcWidth.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]srcIncrementAmount to increment/decrement the DMA source address by. One of DL_DMA_INCREMENT.
See also
DL_DMA_configTransfer
DL_DMA_setSrcAddr
DL_DMA_setSrcWidth

References DL_Common_updateReg().

§ DL_DMA_getSrcIncrement()

__STATIC_INLINE DL_DMA_INCREMENT DL_DMA_getSrcIncrement ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Return a channel's source address increment amount.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
The source address increment amount for selected channel
Return values
Oneof DL_DMA_INCREMENT.

§ DL_DMA_setDestIncrement()

__STATIC_INLINE void DL_DMA_setDestIncrement ( DMA_Regs *  dma,
uint8_t  channelNum,
DL_DMA_INCREMENT  destIncrement 
)

Set a channel's destination address increment amount.

After each DMA transfer the channel destination address, which can be set by DL_DMA_setDestAddr, can be incremented, decremented or remain unchanged. This controls if the DMA is copying from a fixed address or a block of addresses.

The amount that is incremented/decremented is controlled by the width of the destination, set by DL_DMA_setDestWidth.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]destIncrementAmount to increment/decrement the DMA destination address by. One of DL_DMA_INCREMENT.
See also
DL_DMA_configTransfer
DL_DMA_setDestAddr
DL_DMA_setDestWidth

References DL_Common_updateReg().

§ DL_DMA_getDestIncrement()

__STATIC_INLINE DL_DMA_INCREMENT DL_DMA_getDestIncrement ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Return a channel's destination address increment amount.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
The destination address increment amount for selected channel
Return values
Oneof DL_DMA_INCREMENT.

§ DL_DMA_setSrcWidth()

__STATIC_INLINE void DL_DMA_setSrcWidth ( DMA_Regs *  dma,
uint8_t  channelNum,
DL_DMA_WIDTH  srcWidth 
)

Set the width of the DMA source address for a channel.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]srcWidthThe width of the DMA source. One of DL_DMA_WIDTH.
See also
DL_DMA_configTransfer

References DL_Common_updateReg().

§ DL_DMA_getSrcWidth()

__STATIC_INLINE DL_DMA_WIDTH DL_DMA_getSrcWidth ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Get the width of the DMA source address for a channel.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
The width of the DMA source for selected channel
Return values
Oneof DL_DMA_WIDTH.

§ DL_DMA_setDestWidth()

__STATIC_INLINE void DL_DMA_setDestWidth ( DMA_Regs *  dma,
uint8_t  channelNum,
DL_DMA_WIDTH  destWidth 
)

Set the width of the DMA destination address for a channel.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]destWidthThe width of the DMA destination. One of DL_DMA_WIDTH.
See also
DL_DMA_configTransfer

References DL_Common_updateReg().

§ DL_DMA_getDestWidth()

__STATIC_INLINE DL_DMA_WIDTH DL_DMA_getDestWidth ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Get the width of the DMA destination address for a channel.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
The width of the DMA destination for selected channel
Return values
Oneof DL_DMA_WIDTH.

§ DL_DMA_Full_Ch_setEarlyInterruptThreshold()

__STATIC_INLINE void DL_DMA_Full_Ch_setEarlyInterruptThreshold ( DMA_Regs *  dma,
uint8_t  channelNum,
DL_DMA_EARLY_INTERRUPT_THRESHOLD  threshold 
)

Set the early interrupt event.

This functionality is available for FULL-channel configuration only. Please refer to the device datasheet to map which channels have FULL or BASIC capability.

The DMA has the capability to generate an early interrupt with a given amount of transfer cycles before the DMA complete-interrupt is issued. This allows to start the ISR context switch in parallel with the completion of the DMA, and compensates the latency for the task switch into the ISR.

Ideally when the ISR starts to execute and read IIDX, the IIDX will already point to the channel-complete interrupt (always higher priority than the PRE-IRQ). In this case the latency is minimal and the ISR needs to clear the PRE-IRQ interrupt flag (RIS) manually. Should for whatever reason the DMA not complete in time, the IIDX will point to the PRE-IRQ handler and the handler needs to poll for the DMAEN bit in the DMA channel control register (DMACTL) to catch the moment that the DMA transfer has completed. Then the handler needs to clear the DMA channel-complete IRQ flag manually.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
[in]thresholdWhen to generate the early interrupt. One of DL_DMA_EARLY_INTERRUPT_THRESHOLD.

References DL_Common_updateReg().

§ DL_DMA_Full_Ch_getEarlyInterruptThreshold()

__STATIC_INLINE DL_DMA_EARLY_INTERRUPT_THRESHOLD DL_DMA_Full_Ch_getEarlyInterruptThreshold ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Get the early interrupt event threshold.

This functionality is available for FULL-channel configuration only. Please refer to the device datasheet to map which channels have FULL or BASIC capability.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
The early interrupt event threshold
Return values
Oneof DL_DMA_EARLY_INTERRUPT_THRESHOLD.

§ DL_DMA_enableInterrupt()

__STATIC_INLINE void DL_DMA_enableInterrupt ( DMA_Regs *  dma,
uint32_t  interruptMask 
)

Enable DMA interrupts.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to enable. Bitwise OR of DL_DMA_INTERRUPT.

§ DL_DMA_disableInterrupt()

__STATIC_INLINE void DL_DMA_disableInterrupt ( DMA_Regs *  dma,
uint32_t  interruptMask 
)

Disable DMA interrupts.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to disable. Bitwise OR of DL_DMA_INTERRUPT.

§ DL_DMA_getEnabledInterrupts()

__STATIC_INLINE uint32_t DL_DMA_getEnabledInterrupts ( const DMA_Regs *  dma,
uint32_t  interruptMask 
)

Check which DMA interrupts are enabled.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to check. Bitwise OR of DL_DMA_INTERRUPT.
Returns
Which of the requested DMA interrupts are enabled
Return values
BitwiseOR of DL_DMA_INTERRUPT values

§ DL_DMA_getEnabledInterruptStatus()

__STATIC_INLINE uint32_t DL_DMA_getEnabledInterruptStatus ( const DMA_Regs *  dma,
uint32_t  interruptMask 
)

Check interrupt flag of enabled DMA interrupts.

Checks if any of the DMA interrupts that were previously enabled are pending.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to check. Bitwise OR of DL_DMA_INTERRUPT.
Returns
Which of the requested DMA interrupts are pending
Return values
BitwiseOR of DL_DMA_INTERRUPT values
See also
DL_DMA_enableInterrupt

§ DL_DMA_getRawInterruptStatus()

__STATIC_INLINE uint32_t DL_DMA_getRawInterruptStatus ( const DMA_Regs *  dma,
uint32_t  interruptMask 
)

Check interrupt flag of any DMA interrupt.

Checks if any of the DMA interrupts are pending. Interrupts do not have to be previously enabled.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to check. Bitwise OR of DL_DMA_INTERRUPT.
Returns
Which of the requested DMA interrupts are pending
Return values
BitwiseOR of DL_DMA_INTERRUPT values

§ DL_DMA_getPendingInterrupt()

__STATIC_INLINE DL_DMA_EVENT_IIDX DL_DMA_getPendingInterrupt ( const DMA_Regs *  dma)

Get highest priority pending DMA interrupt.

Checks if any of the DMA interrupts are pending. Interrupts do not have to be previously enabled.

Parameters
[in]dmaPointer to the register overlay for the peripheral
Returns
The highest priority pending DMA interrupt
Return values
Oneof DL_DMA_EVENT_IIDX

§ DL_DMA_clearInterruptStatus()

__STATIC_INLINE void DL_DMA_clearInterruptStatus ( DMA_Regs *  dma,
uint32_t  interruptMask 
)

Clear pending DMA interrupts.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to clear. Bitwise OR of DL_DMA_INTERRUPT.

§ DL_DMA_setPublisherChanID()

__STATIC_INLINE void DL_DMA_setPublisherChanID ( DMA_Regs *  dma,
DL_DMA_PUBLISHER_INDEX  index,
uint8_t  chanID 
)

Sets the event publisher channel id.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
[in]chanIDChannel ID number. Valid range 0-15. If ChanID == 0 publisher is disconnected.

§ DL_DMA_getPublisherChanID()

__STATIC_INLINE uint8_t DL_DMA_getPublisherChanID ( DMA_Regs *  dma,
DL_DMA_PUBLISHER_INDEX  index 
)

Gets the event publisher channel id.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
Returns
Event publisher channel ID

§ DL_DMA_setSubscriberChanID()

__STATIC_INLINE void DL_DMA_setSubscriberChanID ( DMA_Regs *  dma,
DL_DMA_SUBSCRIBER_INDEX  index,
uint8_t  chanID 
)

Sets the event subscriber channel id.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
[in]chanIDChannel ID number. Valid range 0-15. If ChanID == 0 subscriber is disconnected.

§ DL_DMA_getSubscriberChanID()

__STATIC_INLINE uint8_t DL_DMA_getSubscriberChanID ( DMA_Regs *  dma,
DL_DMA_SUBSCRIBER_INDEX  index 
)

Gets the event subscriber channel id.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
Returns
Event subscriber channel ID

§ DL_DMA_enableEvent()

__STATIC_INLINE void DL_DMA_enableEvent ( DMA_Regs *  dma,
uint32_t  eventMask 
)

Enable DMA event.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]eventMaskBit mask of events to enable. Bitwise OR of DL_DMA_EVENT.

§ DL_DMA_disableEvent()

__STATIC_INLINE void DL_DMA_disableEvent ( DMA_Regs *  dma,
uint32_t  eventMask 
)

Disable DMA event.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]eventMaskBit mask of events to enable. Bitwise OR of DL_DMA_EVENT.

§ DL_DMA_getEnabledEvents()

__STATIC_INLINE uint32_t DL_DMA_getEnabledEvents ( const DMA_Regs *  dma,
uint32_t  eventMask 
)

Check which dma events triggers are enabled.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]eventMaskBit mask of events to check. Bitwise OR of DL_DMA_EVENT.
Returns
Which of the requested dma events are enabled
Return values
BitwiseOR of DL_DMA_EVENT values

§ DL_DMA_getEnabledEventStatus()

__STATIC_INLINE uint32_t DL_DMA_getEnabledEventStatus ( const DMA_Regs *  dma,
uint32_t  eventMask 
)

Check event flag of enabled dma event.

Checks if any of the dma events that were previously enabled are pending.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]eventMaskBit mask of events to check. Bitwise OR of DL_DMA_EVENT.
Returns
Which of the requested dma events are pending
Return values
BitwiseOR of DL_DMA_EVENT values
See also
DL_DMA_enableEvent

§ DL_DMA_getRawEventsStatus()

__STATIC_INLINE uint32_t DL_DMA_getRawEventsStatus ( const DMA_Regs *  dma,
uint32_t  eventMask 
)

Check event flag of any dma event.

Checks if any events are pending. Events do not have to be previously enabled.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]eventMaskBit mask of event to check. Bitwise OR of DL_DMA_EVENT.
Returns
Which of the requested dma event are pending
Return values
BitwiseOR of DL_DMA_EVENT values

§ DL_DMA_clearEventsStatus()

__STATIC_INLINE void DL_DMA_clearEventsStatus ( DMA_Regs *  dma,
uint32_t  eventMask 
)

Clear pending dma events.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]eventMaskBit mask of events to clear. Bitwise OR of DL_DMA_EVENT.

§ DL_DMA_enableAutoEnable()

__STATIC_INLINE void DL_DMA_enableAutoEnable ( DMA_Regs *  dma,
DL_DMA_AUTOEN  mode,
uint8_t  channelNum 
)

Configure the DMA for auto-enable.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]modeEnable auto-enable for DMA on a specified register write. One of DL_DMA_AUTOEN
[in]channelNumDMA channel to operate on

§ DL_DMA_disableAutoEnable()

__STATIC_INLINE void DL_DMA_disableAutoEnable ( DMA_Regs *  dma,
uint8_t  channelNum 
)

Disable auto-enable for DMA.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on

§ DL_DMA_isAutoEnableEnabled()

__STATIC_INLINE bool DL_DMA_isAutoEnableEnabled ( const DMA_Regs *  dma,
uint8_t  channelNum 
)

Check if auto-enable is enabled for the DMA.

Parameters
[in]dmaPointer to the register overlay for the peripheral
[in]channelNumDMA channel to operate on
Returns
The status of auto-enable
Return values
trueauto-enable is enabled
falseauto-enable is disabled
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale