MSPM0GX51X Driver Library  2.05.01.00
Macros
Collaboration diagram for DL_TIMERG_INTERRUPT:

Macros

#define DL_TIMERG_INTERRUPT_ZERO_EVENT   (DL_TIMER_INTERRUPT_ZERO_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_ZERO_EVENT.
 
#define DL_TIMERG_INTERRUPT_LOAD_EVENT   (DL_TIMER_INTERRUPT_LOAD_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_LOAD_EVENT.
 
#define DL_TIMERG_INTERRUPT_CC0_DN_EVENT   (DL_TIMER_INTERRUPT_CC0_DN_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_CC0_DN_EVENT.
 
#define DL_TIMERG_INTERRUPT_CC1_DN_EVENT   (DL_TIMER_INTERRUPT_CC1_DN_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_CC1_DN_EVENT.
 
#define DL_TIMERG_INTERRUPT_CC0_UP_EVENT   (DL_TIMER_INTERRUPT_CC0_UP_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_CC0_UP_EVENT.
 
#define DL_TIMERG_INTERRUPT_CC1_UP_EVENT   (DL_TIMER_INTERRUPT_CC1_UP_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_CC1_UP_EVENT.
 
#define DL_TIMERG_INTERRUPT_CC2_DN_EVENT   (DL_TIMER_INTERRUPT_CC2_DN_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_CC2_DN_EVENT. More...
 
#define DL_TIMERG_INTERRUPT_CC3_DN_EVENT   (DL_TIMER_INTERRUPT_CC3_DN_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_CC3_DN_EVENT. More...
 
#define DL_TIMERG_INTERRUPT_CC2_UP_EVENT   (DL_TIMER_INTERRUPT_CC2_UP_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_CC2_UP_EVENT. More...
 
#define DL_TIMERG_INTERRUPT_CC3_UP_EVENT   (DL_TIMER_INTERRUPT_CC3_UP_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_CC3_UP_EVENT. More...
 
#define DL_TIMERG_INTERRUPT_OVERFLOW_EVENT   (DL_TIMER_INTERRUPT_OVERFLOW_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_OVERFLOW_EVENT.
 
#define DL_TIMERG_INTERRUPT_DC_EVENT   (DL_TIMER_INTERRUPT_DC_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_DC_EVENT. More...
 
#define DL_TIMERG_INTERRUPT_QEI_ERR_EVENT   (DL_TIMER_INTERRUPT_QEIERR_EVENT)
 Redirects to common DL_TIMER_INTERRUPT_QEIERR_EVENT. More...
 

Detailed Description

Macro Definition Documentation

§ DL_TIMERG_INTERRUPT_CC2_DN_EVENT

#define DL_TIMERG_INTERRUPT_CC2_DN_EVENT   (DL_TIMER_INTERRUPT_CC2_DN_EVENT)

Redirects to common DL_TIMER_INTERRUPT_CC2_DN_EVENT.

Note
This interrupt is only available on some TimerG variants with 4 external CCP Channels. Please refer to "TIMx Configurations" table in the device specific datasheet.

§ DL_TIMERG_INTERRUPT_CC3_DN_EVENT

#define DL_TIMERG_INTERRUPT_CC3_DN_EVENT   (DL_TIMER_INTERRUPT_CC3_DN_EVENT)

Redirects to common DL_TIMER_INTERRUPT_CC3_DN_EVENT.

Note
This interrupt is only available on some TimerG variants with 4 external CCP Channels. Please refer to "TIMx Configurations" table in the device specific datasheet.

§ DL_TIMERG_INTERRUPT_CC2_UP_EVENT

#define DL_TIMERG_INTERRUPT_CC2_UP_EVENT   (DL_TIMER_INTERRUPT_CC2_UP_EVENT)

Redirects to common DL_TIMER_INTERRUPT_CC2_UP_EVENT.

Note
This interrupt is only available on some TimerG variants with 4 external CCP Channels. Please refer to "TIMx Configurations" table in the device specific datasheet.

§ DL_TIMERG_INTERRUPT_CC3_UP_EVENT

#define DL_TIMERG_INTERRUPT_CC3_UP_EVENT   (DL_TIMER_INTERRUPT_CC3_UP_EVENT)

Redirects to common DL_TIMER_INTERRUPT_CC3_UP_EVENT.

Note
This interrupt is only available on some TimerG variants with 4 external CCP Channels. Please refer to "TIMx Configurations" table in the device specific datasheet.

§ DL_TIMERG_INTERRUPT_DC_EVENT

#define DL_TIMERG_INTERRUPT_DC_EVENT   (DL_TIMER_INTERRUPT_DC_EVENT)

Redirects to common DL_TIMER_INTERRUPT_DC_EVENT.

Note
This interrupt is only available on some TimerG variants with Quadrature Encoding Input (QEI). Please refer to "TIMx Configurations" table in the device specific datasheet.

§ DL_TIMERG_INTERRUPT_QEI_ERR_EVENT

#define DL_TIMERG_INTERRUPT_QEI_ERR_EVENT   (DL_TIMER_INTERRUPT_QEIERR_EVENT)

Redirects to common DL_TIMER_INTERRUPT_QEIERR_EVENT.

Note
This interrupt is only available on some TimerG variants with Quadrature Encoding Input (QEI). Please refer to "TIMx Configurations" table in the device specific datasheet.
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale