MSPM0C110X Driver Library  2.05.01.00
Data Fields
DL_DMA_Config Struct Reference

Configuration struct for DL_DMA_initChannel. More...

#include <dl_dma.h>

Data Fields

uint8_t trigger
 
DL_DMA_TRIGGER_TYPE triggerType
 
DL_DMA_TRANSFER_MODE transferMode
 
DL_DMA_EXTENDED_MODE extendedMode
 
DL_DMA_WIDTH srcWidth
 
DL_DMA_WIDTH destWidth
 
DL_DMA_INCREMENT srcIncrement
 
DL_DMA_INCREMENT destIncrement
 

Detailed Description

Configuration struct for DL_DMA_initChannel.

Field Documentation

§ trigger

uint8_t DL_DMA_Config::trigger

The event that should trigger a DMA transfer. Refer to the datasheet of the device for which DMA trigger values map to which events.

§ triggerType

DL_DMA_TRIGGER_TYPE DL_DMA_Config::triggerType

Configure whether the DMA selects an internal or external channel as the DMA trigger

§ transferMode

DL_DMA_TRANSFER_MODE DL_DMA_Config::transferMode

The transfer mode to use. Refer to the device datasheet to determine which modes are supported in the selected channel. One of DL_DMA_TRANSFER_MODE.

§ extendedMode

DL_DMA_EXTENDED_MODE DL_DMA_Config::extendedMode

The extended mode to use. One of DL_DMA_EXTENDED_MODE.

§ srcWidth

DL_DMA_WIDTH DL_DMA_Config::srcWidth

The width of the DMA source. One of DL_DMA_WIDTH.

§ destWidth

DL_DMA_WIDTH DL_DMA_Config::destWidth

The width of the DMA destination. One of DL_DMA_WIDTH.

§ srcIncrement

DL_DMA_INCREMENT DL_DMA_Config::srcIncrement

Amount to increment/decrement the DMA source address by. One of DL_DMA_INCREMENT.

§ destIncrement

DL_DMA_INCREMENT DL_DMA_Config::destIncrement

Amount to increment/decrement the DMA destination address by. One of DL_DMA_INCREMENT.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale