MSPM0C110X Driver Library  2.05.01.00
Macros
Collaboration diagram for DL_UART_DMA_INTERRUPT_RX:

Macros

#define DL_UART_DMA_INTERRUPT_RX   (UART_DMA_TRIG_RX_IMASK_RXINT_SET)
 UART interrupt for enabling UART receive as DMA trigger.
 
#define DL_UART_DMA_DONE_INTERRUPT_RX   (UART_CPU_INT_IMASK_DMA_DONE_RX_SET)
 UART interrupt indicating DMA is done with the RX.
 
#define DL_UART_DMA_INTERRUPT_RX_TIMEOUT   (UART_DMA_TRIG_RX_IMASK_RTOUT_SET)
 UART interrupt for enabling UART receive timeout as DMA trigger.
 

Detailed Description

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale