![]() |
![]() |
|
MSPM0C1105_C1106 Driver Library
2.05.01.00
|
Configuration struct for DL_DMA_initChannel. More...
#include <dl_dma.h>
Configuration struct for DL_DMA_initChannel.
| uint8_t DL_DMA_Config::trigger |
The event that should trigger a DMA transfer. Refer to the datasheet of the device for which DMA trigger values map to which events.
| DL_DMA_TRIGGER_TYPE DL_DMA_Config::triggerType |
Configure whether the DMA selects an internal or external channel as the DMA trigger
| DL_DMA_TRANSFER_MODE DL_DMA_Config::transferMode |
The transfer mode to use. Refer to the device datasheet to determine which modes are supported in the selected channel. One of DL_DMA_TRANSFER_MODE.
| DL_DMA_EXTENDED_MODE DL_DMA_Config::extendedMode |
The extended mode to use. One of DL_DMA_EXTENDED_MODE.
| DL_DMA_WIDTH DL_DMA_Config::srcWidth |
The width of the DMA source. One of DL_DMA_WIDTH.
| DL_DMA_WIDTH DL_DMA_Config::destWidth |
The width of the DMA destination. One of DL_DMA_WIDTH.
| DL_DMA_INCREMENT DL_DMA_Config::srcIncrement |
Amount to increment/decrement the DMA source address by. One of DL_DMA_INCREMENT.
| DL_DMA_INCREMENT DL_DMA_Config::destIncrement |
Amount to increment/decrement the DMA destination address by. One of DL_DMA_INCREMENT.