MSPM0G3507SensorlessFOCMotorControlLibrary  1.0
Data Fields
userInputRvrDrvCfg Struct Reference

userInputRvrDrvCfg structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t activeBrakeKi: 10
 
uint32_t activeBrakeKp: 10
 
uint32_t revDrvOpenLoopAccelA2: 4
 
uint32_t revDrvOpenLoopAccelA1: 4
 
uint32_t revDrvConfig: 1
 
uint32_t reserved: 3
 

Detailed Description

userInputRvrDrvCfg structure

Field Documentation

§ activeBrakeKi

uint32_t userInputRvrDrvCfg::activeBrakeKi

active braking loop Ki

Referenced by update_RvsDrvConfig().

§ activeBrakeKp

uint32_t userInputRvrDrvCfg::activeBrakeKp

active braking loop Kp

Referenced by update_RvsDrvConfig().

§ revDrvOpenLoopAccelA2

uint32_t userInputRvrDrvCfg::revDrvOpenLoopAccelA2

Open loop acceleration coefficient A2 during reverse drive

Referenced by update_RvsDrvConfig().

§ revDrvOpenLoopAccelA1

uint32_t userInputRvrDrvCfg::revDrvOpenLoopAccelA1

Open loop acceleration coefficient A1 during reverse drive

Referenced by update_RvsDrvConfig().

§ revDrvConfig

uint32_t userInputRvrDrvCfg::revDrvConfig

Chooses between forward and reverse drive setting for reverse drive

Referenced by update_RvsDrvConfig().

§ reserved

uint32_t userInputRvrDrvCfg::reserved

Reserved


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale