MSPM0G3507SensorlessFOCMotorControlLibrary  1.0
Data Fields
userInputFaultCfg1 Struct Reference

userInputFaultCfg1 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t mtrLckMode: 2
 
uint32_t lockRetry: 4
 
uint32_t reserved: 26
 

Detailed Description

userInputFaultCfg1 structure

Field Documentation

§ mtrLckMode

uint32_t userInputFaultCfg1::mtrLckMode

Motor Lock Mode

§ lockRetry

uint32_t userInputFaultCfg1::lockRetry

Lock detection retry time

§ reserved

uint32_t userInputFaultCfg1::reserved

Reserved


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale