![]() |
![]() |
MSPM0G3507SensorlessFOCMotorControlLibrary
1.0
|
ramAlgoDebugCtrl1 structure More...
#include <appInputCtrlInterface.h>
Data Fields | |
uint32_t | reserved1: 10 |
uint32_t | forceAlignAngleSrcSelect: 1 |
uint32_t | forceISDEn: 1 |
uint32_t | forceIPDEn: 1 |
uint32_t | forceSlowCycleFirstCycleEn: 1 |
uint32_t | forceAlignEn: 1 |
uint32_t | closeLoopDis: 1 |
uint32_t | reserved: 6 |
uint32_t | forcedAlignAngle: 9 |
uint32_t | clearFlt: 1 |
ramAlgoDebugCtrl1 structure
uint32_t ramAlgoDebugCtrl1::reserved1 |
Reserved
uint32_t ramAlgoDebugCtrl1::forceAlignAngleSrcSelect |
Force align angle state source select
uint32_t ramAlgoDebugCtrl1::forceISDEn |
Force ISD enable
uint32_t ramAlgoDebugCtrl1::forceIPDEn |
Force IPD enable
uint32_t ramAlgoDebugCtrl1::forceSlowCycleFirstCycleEn |
Force slow first cycle enable
uint32_t ramAlgoDebugCtrl1::forceAlignEn |
Force align state enable
uint32_t ramAlgoDebugCtrl1::closeLoopDis |
Disable closed loop
uint32_t ramAlgoDebugCtrl1::reserved |
Reserved
uint32_t ramAlgoDebugCtrl1::forcedAlignAngle |
Align angle used during forced align state
uint32_t ramAlgoDebugCtrl1::clearFlt |
Clears all faults