![]() |
![]() |
|
MSPM0G3519SensoredFOCMotorControlLibrary
1.0
|
#include "brake.h"#include "stdint.h"#include "softStop.h"#include "measure.h"#include "triState.h"

Go to the source code of this file.
Data Structures | |
| union | LOAD_FLAGS_T |
| Load Flags Working Structure. More... | |
| struct | LOAD_FLAGS_T::loadFlags |
| Load Flags Struct. More... | |
| struct | LOAD_T |
| Load Working Structure. More... | |
Enumerations | |
| enum | LOAD_STATE_TYPES { LOAD_INIT = 0, LOAD_TRISTATE = 1, LOAD_BRAKE = 2, LOAD_START = 3, LOAD_RUN = 4, LOAD_STOP_INIT = 5, LOAD_SOFT_STOP = 6, LOAD_STOP = 7, LOAD_FAULT = 8, LOAD_ALIGN_STOP = 9 } |
| Load State Machine Values. More... | |
| enum | LOAD_FAULT_TYPES { LOAD_NO_FAULT = 0 } |
| Load Fault Values. More... | |
Functions | |
| void | loadInit (LOAD_T *pLoad) |
| Load Init. More... | |
| void | loadRun (LOAD_T *pLoad) |
| Load Run. More... | |
| void | loadLowPriorityRun (LOAD_T *pLoad) |
| Load Low Priority Run. More... | |
| _Bool | getLoadStartReadyStatus (LOAD_T *pLoad) |
| LoadStartReadyStatus Status check. More... | |
| _Bool | getLoadStopReadyStatus (LOAD_T *pLoad) |
| Load Stop Status check. More... | |
| _Bool | getLoadStallStatus (LOAD_T *pLoad) |
| Load Stall Status check. More... | |
| _Bool | runMotorDuringStop (LOAD_T *pLoad) |
| Motor Run Status check. More... | |
| enum LOAD_STATE_TYPES |
Load State Machine Values.
| enum LOAD_FAULT_TYPES |
| void loadInit | ( | LOAD_T * | pLoad | ) |
Load Init.
| [in] | *pLoad | Input Pointer |
References LOAD_FLAGS_T::b, BRAKE_FLAGS_T::b, LOAD_T::brake, brakeInit(), BRAKE_FLAGS_T::brakeFlags::enableOnStop, FALSE, BRAKE_T::flags, LOAD_T::flags, LOAD_FLAGS_T::loadFlags::loadStartReadyStatus, LOAD_FLAGS_T::loadFlags::loadStopReadyStatus, SOFT_STOP_T::minimumSpeed, SOFT_STOP_T::minimumSpeedBrake, SOFT_STOP_T::minimumSpeedSoftStop, LOAD_T::softStop, softStopInit(), LOAD_T::triState, and triStateInit().
Referenced by loadRun().
| void loadRun | ( | LOAD_T * | pLoad | ) |
Load Run.
| [in] | *pLoad | Input Pointer |
References SOFT_STOP_FLAGS_T::b, LOAD_FLAGS_T::b, BRAKE_FLAGS_T::b, MEASURE_CURRENT_FLAGS_T::b, LOAD_T::brake, BRAKE_FLAGS_T::brakeFlags::brakeCheckCurrentFault, BRAKE_FLAGS_T::brakeFlags::brakeCheckCurrentStart, BRAKE_FLAGS_T::brakeFlags::brakeCheckCurrentStop, BRAKE_FLAGS_T::brakeFlags::brakeCheckOnCurrent, brakeInit(), BRAKE_FLAGS_T::brakeFlags::brakeOnStart, brakeRun(), HAL_MEASURE_MOTOR_INPUTS_T::current, HAL_MEASURE_CURRENT_T::currentShunt, SOFT_STOP_FLAGS_T::softStopFlags::enable, SOFT_STOP_FLAGS_T::softStopFlags::enableOnBrake, BRAKE_FLAGS_T::brakeFlags::enableOnFault, BRAKE_FLAGS_T::brakeFlags::enableOnStart, BRAKE_FLAGS_T::brakeFlags::enableOnStop, FALSE, SOFT_STOP_T::flags, BRAKE_T::flags, LOAD_T::flags, HAL_MEASURE_CURRENT_T::flags, getBrakeStatusCurrent(), getBrakeStatusTimeOut(), getSoftStopStatus(), getTriStateStatus(), HAL_EnableLowSideBrake(), HAL_SetPhaseCurrentChannels(), LOAD_BRAKE, LOAD_FAULT, LOAD_INIT, LOAD_RUN, LOAD_SOFT_STOP, LOAD_START, LOAD_STOP, LOAD_STOP_INIT, LOAD_TRISTATE, loadInit(), LOAD_FLAGS_T::loadFlags::loadStartReadyStatus, LOAD_FLAGS_T::loadFlags::loadStopReadyStatus, LOAD_T::pMotorInputs, LOAD_T::softStop, softStopRun(), LOAD_T::state, measureCurrentFlags::threeShuntDynamic, BRAKE_T::timeOutCountMax, BRAKE_T::timeOutCountMaxOnStart, BRAKE_T::timeOutCountMaxOnStop, LOAD_T::triState, and TRUE.
| void loadLowPriorityRun | ( | LOAD_T * | pLoad | ) |
Load Low Priority Run.
| [in] | *pLoad | Input Pointer |
References LOAD_T::brake, brakeLowPriorityRun(), LOAD_BRAKE, LOAD_TRISTATE, LOAD_T::state, LOAD_T::triState, and triStateRun().
|
inline |
LoadStartReadyStatus Status check.
| [in] | *pLoad | Pointer |
References LOAD_FLAGS_T::b, LOAD_T::flags, and LOAD_FLAGS_T::loadFlags::loadStartReadyStatus.
|
inline |
Load Stop Status check.
| [in] | *pLoad | Pointer |
References LOAD_FLAGS_T::b, LOAD_T::flags, and LOAD_FLAGS_T::loadFlags::loadStopReadyStatus.
|
inline |
Load Stall Status check.
| [in] | *pLoad | Pointer |
References LOAD_T::faultStatus, and LOAD_NO_FAULT.
|
inline |
Motor Run Status check.
| [in] | *pLoad | Pointer |
References LOAD_ALIGN_STOP, LOAD_SOFT_STOP, LOAD_STOP_INIT, and LOAD_T::state.